Other Parts Discussed in Thread: AMC1305M25 , AMC1304M25 , ADS1118 , ADS1248 , TMS320F28377D , ADS5560 , ADS1610 , ADS5562 , AMC1210 HI,
I'm interested in the AMC1305M25 ADC chip, I'm hoping to achieve 16bit resolution at 20 MSps data conversion using this chip…
Other Parts Discussed in Thread: ADS5562 , ADS5560 Hello,
I am having an issue using the external trigger on the TSW1400EVM. The external trigger only works about 75% of the time and I have spent hours trying to debug whether this is an issue with the High…
Bill,
The ADS5560 will be able to handle standard LVPECL input swings. You can follow the standard LVPECL termination between the clock chip output and the ADS5560 clock input. It is the same as your circuit based on your description above.
The absolute…
Thanks, but as I said, I prefer to keep it below 100MHz. I ran across these today.
ADS5560 or ADS5562 ADC and TSW1200 Capture Board
Mustly I need good access to the input amplfiers, power supplies, voltage reference and clock . The goal is to assess the…
Other Parts Discussed in Thread: ADS5560 I am looking for a specifiction document for the ADS5560 which might give information like Analog input range/impdeance/bandwidth. I also need something for the clock input as well.
Hi Lee,
I suggest searching for a 16-bit high speed ADC. The ADS5560 would be another device to investigate.
Since I'm not as familiar with high-speed applications, I am moving your topic to the high speed data converter forum. Perhaps that group will…
I have the same problem as Bram mentioned in his recent post, with a newly purchased Rev C ADS5560 EVM board and no current schematic available from TI. There must be a substantial change to this schematic too because upon preliminary investigation I…
Other Parts Discussed in Thread: ADS5560 , ADS6149 , FMC-ADC-ADAPTER , ADS5560EVM ADS61x9/55xxEVM User's Guide (June 2009) does not show the connections from the ADS5560 (16-bit ADC) to the J10 connector. The schematic shows for instance, that 'D0_D1…
Hello Peter,
I have confirmed with the design team that the ADS5560/62 has SCLK pin function as below:
SCLK pin functions as below:
SCLK voltage
Function
0
Gain 3dB, Low Speed Mode Disable
DRVDD
Gain 1dB…
Hi Richard,
In my new design I am going to interface ADS5560 to Spartan 6. Could you send me the Verilog code for TSW1200 to my email ( lizakarn@gmail.com ) so I can use it as a reference?
Thanks a lot.
Zak.