Part Number: ADS5560
Our KMM customers encounter the following questions during the use of ads5560. Please help to answer them
1、 Whether the clock can adopt the differential clock output by FPGA, or still have to use a special clock chip to form a fully…
Hi Chunqi lv, Sorry for the delay in my response due to holidays.
What is the clock frequency you are using? 40MHz?
Did you evaluate an ADS5560EVM or working on a custom board for you use-case?
I can't think of a reason why the output clock duty cycle…
Part Number: TSW1400EVM Dear TI expert,
I am investigating TSW14xx for a DAQ project, in the slwu087d.pdf. page 16, 3.1.3. trigger operation.
"Clicking on the Trigger Option will open a new panel as shown in Figure 12. This option is not available for…
Hello Kang,
I came across this posting after searching for information regarding the ADS5560EVM using its CMOS output mode. I need to design an interface to the EMV for this CMOS data output, but the schematic supplied from User's Guide SLAU260-December…
Other Parts Discussed in Thread: ADS5560EVM , TUSB3410 Hello,
I hve just gotten my TSW1200 and ADS5560EVM boards and was trying to set up the TSW1200 first but after I installed the software from the enclosed CD and attached the USB cable then powered…
Jin,
The schematic looks good for the most part. Please do the following:
1. Install R364 to provide a path to GND.
2. Do not use R361, R362, and R363 wit the ADC_VCM output.
3. Make sure DRVDD and AVDD are 3.3V.
4. Do not need to route ADC_CLKOUTM_F if…
Other Parts Discussed in Thread: ADS5560 Hello Engineers,
Using the ADS5560 EVM, I am trying to reproduce the results shown on page 27 of the datasheet for the ADS5560 chip. The image below shows the output spectrum I generated with a 2 MHz input tone…