Hi Amy,
Just FYI, the configuration that I used to capture all pattern is below:
testC48.txt
00 x00
25 x00
2B x00
31 x00
37 x00
3D x00
41 x00
42 x08
44 x01
45 x00
26 x00
28 x40
2D x00
2E …
Hi HY yang,
This is likely a timing issue in the fpga since it fails only at high speed. I will recommend you check that there are no timing violations on the LVDS bus.
Thanks,
Eben.
Part Number: ADS58C48 Hi ,
I am designing a system which is based on the design of TSW1200 with ADS58C48EVM . I need a reference. Would you provide me the verilog source code for my reference?
My email: luojiulin1013@sina.cn
Sincerely,
J.L. Luo
Part Number: ADS6423 Other Parts Discussed in Thread: ADS58C48 , ADS4249 Hi,
We are designing a 4 channel data capture system as below: Minimum slew rate of signal = 300 ns; sample time minimum 30 ns; 11 bit resolution;
12 samples = 25 ns; 40 MSPS per…
the hsmc-adc-bridge REV c does not support ADS58C48EVM Channel A or Channel B outputs, it connects them to ground.
Will connecting these outputs to ground damage the ADS58C48?
Do I need a hsmc_adc_bridge REV B that supports Channel A and B without grounding…
Other Parts Discussed in Thread: ADS58C48 , ADS58C48EVM , TSW1200EVM Hello, I'm trying to use your ADS58C48 adc in an experiment I'm involved in. I am using the ADS58C48EVM to try and figure out the output data format. I'm confused by the ADS58C48…
Other Parts Discussed in Thread: ADS58C48EVM , ADS58C48 , TSW1200EVM Hello forum,
I'm working with the TI ADS58c48EVM attached to TI TSW1200EVM to evaluate the ADS58c48's performance for a project. I followed the ADS58c48EVM User's Guide, pgs 6-8…
Other Parts Discussed in Thread: THS4509 , ADS58C48 , TEST , ADS5517 Hi,
I am debugging a customized board. It's a high speed data acquisition card with THS4509+ADS58C48+FPGA.
The amplifier is THS4509 set as 20dB gain. And ADC is ADS58C48. Four channels…
Other Parts Discussed in Thread: ADS58C48 , ADS58C48EVM Hi,
I'm using ADS58C48 EVM and ADS58C48 EVM software control. And I know I can configure ADC via software control.
But I have a problem, when I configure ADC via software control and I want to…
Other Parts Discussed in Thread: ADS58C48 Hi
I just want to know if the clock signal input of ADS58C48 EVM can take directly a sine wave or I have to add an circuit before clock input
thanks