Part Number: ADS58J63 Tool/software: Hi team,
This is FAE Jayden, my customer is using ADS58J63 in their wireless infrastructure product. Here're some questions from my customer:
1. How to configure the device to select which mode? Is the mode selection…
Part Number: ADS58J63 Hello, could you please let me know if we can retrieve the PLL lock status through a register? We require this information so that we may automate the process of establishing the sanity of our system.
Part Number: ADS58J63 Hi, I am using ADC ADS58J63 in my design. I want to enable single SYNCb input using SYNCCD for channel A/B and chaneel C/D. I can see in the data sheet of ADS58J63 in page number 71, Table 63 STEP 7.
But register address 7001h…
Part Number: ADS58J63 Hi TI Team,
Greetings for the day.
We are using ADS58J63 in our receiver system.
In DATA sheet Differential input resistance 0.5kE and Differential input capacitance 2.5pF has given. Down converted IF Differential 100E signal…
Part Number: ADS58J63 Hi, I am using ADS58J63 in my design. In the JESD Analog page (6A00h) the bits D1 and D0 shows the JESD PLL MODE settings as in below image (Page number 70 and Figure 136 in data sheet)
But in the Field Descriptions it is mentioned…
Kiran,
These pins are separate internally. But, I would suggest you only use one GND plane. See the attached file for more tips and information regarding layout.
Regards,
Jim
5076.High Speed Serial Link Layout Recommendations.pptx
Part Number: ADS58J63 Other Parts Discussed in Thread: ADS54J20 I downloaded the IBIS-AMI model for ADS58J63. I see two package model files in it namely - tx_package_DA0.s4p and tx_package_DA1.s4p.
I would like to know if these are the actual package…
Part Number: ADS58J63 Hi,
I am using the below given analog input circuit for ADS58J63. I read in one of the forum post suggesting to remove R841, C2946 and R849 if using in 2nd Nyquist zone. Is that suggestion valid for ADS58J63 also?
My sampling…