Part Number: ADS6142-HT We’re considering using the ADS6142 ADC for our design and we wanted a high temperature version, so we found out that there’s ADS6142-HT available too but only in die form.
I wanted know if ADS6142 (non-HT part) uses…
Hello,
ADS6142-HT SLWS234 - December 2011 Datasheet has bond pad numbers 47, 50, 55, 56, 61, 64, 67, 70 and 72 with a description of SUBST. The backside potential is listed as DRVSS. Should the SUBST bond pads be connected to DRVSS along with the backside…
Brian, just to clarify. The ADS6142-HT max. sampling rate is 65 MSPS as stated in p.7 of the datasheet in the "Clock Input" section. The confusion here is because there are some commercial devices (not rated for high temperatures, but with sampling frequencies…