Other Parts Discussed in Thread: ADS62P42 the circuite is almost the same as the reference in the datasheet of ADS62P42IRGCT. it is shown below
when i test the idle noise of the circuite(call it be called "offset"? ).the first channel is about 15,while…
Hi Andrey,
The register maps are located on the following pages of each respective datasheet:
ADS62P28/29/48/49, see page 21
ADS62P22/23/24/25 see page 17
ADS62P42/43/44/45 see page 20
Regards, Matt Guibord
Other Parts Discussed in Thread: ADS62P42 , ADS1675 , REF5025 I can not seem to get the ADS62P42 adc to continue to work. It work just fine for a while but then the outputs stop working. I am using an FPGA to interface with it and thought that perhaps upon…
I found a thread (http://e2e.ti.com/support/dsp/omap_applications_processors/f/42/p/193799/699365.aspx#699365) mentioning the uPP interface to connect to high speed ADCs. This seems to be available with the C674x/OMAP-L1x devices. Could this be a solution…
Other Parts Discussed in Thread: ADS62P43 , TINA-TI , THS5671A , ADS62P42 Hello.
Could any one help me how to get spice model not for simulation only design layout library for ADS62P43.
Dose ti supply spice model's?
A possible combination I've found could be the C28346 experimenters kit and ADS62P42 (I don't need more than 60 MSPS I think). This ADC can also come in an evaluation module. Is this a good way to simplify setup, or is the evaluation module not intended…
Hello.
I am trying to get from you gauys(Ti) for one week an orcade capture .ilb or .lib file with pin layout for THS5671A that i am using in my project and also for ADS62P42
I need only symbolic of this part.
Thx.
Hi George,
Is the customer using the CCD for a medical application? If so, we might need to move the post to the High Reliability forum and they can make a better recommendation that is qualified for medical use.
http://e2e.ti.com/support/applications…
Hi!
I'm connecting an adc to XINTF. Don't want to use any of the xinf signals, just want the DMA to take the data from the bus.
Can I violate the minimum wait state requirements for Lead and Active period in read cycle?
When is the data latched…
Hi Preia,
The 5-6K Interface board will fit on the TMS320C6416 DSK, but that interface board was not really designed to do what you are looking to do. The board breaks out the EMIF found on the memory expansion connector (J4) and the two McBSP ports…