Part Number: ADS62P49 Other Parts Discussed in Thread: CDCE72010 , Dear Sir,
I have made a vivado design on Carrier card Zynq ZC702 and Evaluation board: FMC150 that houses ADS62P49 + CDCE72010. I am uploading my design. The design composes of fmc150_adc_interface…
Part Number: ADS62P49
The datasheet page 10 says that: All digital inputs support 1.8V and 3.3V CMOS logic levels.
Can I use LVCMOS 2.5 logic? I would like to eliminate the use of a superfluous level translator.
Part Number: ADS62P49 We are reviewing "ADS62P49EVM". I'm asking because I think there is something wrong in the circuit schematic.
ADC's Clock Out Pin seems to have the wrong polarity. Please check.
Thank you.
Part Number: ADS62P49 We have designed and tested a board using the ADS62P49. We are digitizing data at 200 MHz, and initial testing showed reasonable results. While integrating this board with our system, we had some issues that caused us to look more…
Part Number: ADS62P49 Offset Correction does not appear to work as stated in the datasheet for the ADC device ADS62P49. We are able to confirm that offset correction is enabled when setting bit 6 of reg 53 to 1. According to pg 64 of datasheet, After…
Part Number: ADS62P49 Hi I am working on a FMC150 card which has ADS62P49 ADC for analog to digital conversion. However, FMC150 datasheet has mentioned the FMC pin layout only in terms of 7 pairs of LVDS _P and _N outputs.
I want to use ADC in LVCMOS…
Part Number: ADS62P49 I am seeing a fixed DC offset in the output of adc when it is set in LVCMOS mode vs when it is set in LVDS output mode. When I give input as sine wave of 10dBm 1MHz frequency, the output of LVCMOS mode is centered at 0 . However…
Part Number: ADS62P49 I am testing the data collection with ADS62P49. When the register is configured according to the register table, it is found that when the input end of AD is suspended, the output collection data of AD is only 0X3FFF and 0x0000.I…
Part Number: ADS62P49 Hi I am using FMC150 card having ADS62p49 on a Xilinx ZC706 board LPC connector. I have provided 10 MHz input and when i see the samples coming out of ADC on ILA of Xilinx, the digital output is sine wave but the amplitude of sine…