Part Number: ADS62P49 Other Parts Discussed in Thread: CDCE62005 HI,
I am using DAC34SH84EVM to provide CLK 250 MHz for the TSW4200-ADC (ADSP62P49).
I am using an Ext CLK 1 GHz at J9 and I got output CLK of 250 MHz at J10 J11. The divided output CLK…
Part Number: ADS62P49 Other Parts Discussed in Thread: ADS4249 Is the ADS62P49 a rigorous enough chip for analog video processing? I am hoping to use the ADC for NTSC video at 30 fps at a resolution of 320x240.
In other words, what are the limits of…
Part Number: ADS62P49 I am trying to simulate Figure 99, which shows a circuit of the input impedance of ADS62P49.
I would expect to get results that are correspond to: Figure 100 and Figure 101, but I seem to be way off.
Other Parts Discussed in Thread: ADS62P49 hello good morning, i would like to ask iwhat does 2's complementary output mean for ADS62P49? does this mean that the outputs are in binary 2's complementary coding scheme where 0000 represents the BPZ?
Part Number: ADS62P49 I have been struggling to get a reliable front end DDR design with FIFOs that will receive data from four separate ADS62P49 ADC driven by a common PLL/clock buffer. I have implemented DDR interfaces using the supplied ADCoutput lane…
Other Parts Discussed in Thread: ADS62P49 , CDCE72010 I'm driving an ADS62P49 CLKP/CLKM with a 20.5 MHz signal, believed to be close to 50% duty ratio. On the CLKOUTP/CLKOUTM, I am getting a 20.5MHz signal with a 13% duty ratio. I have set the Low Speed…
Other Parts Discussed in Thread: ADS62P49 , ADS62P48 Hi TI,
I am using TSW1400 EVM to interface ADS62P49 EVM via CMOS.
Connected CMOS Pin 1 on TSW1400 to pin 39 of ADS 62p49EVM board.
User LED 3 , 4 is not ON in the TSW 1400 board
I want to simply…
Other Parts Discussed in Thread: CDCE72010 , ADS62P49 Hi,
I have a question about the clock path between the LVCMOS driver of the CDCE72010 and the clock buffer of the ADS62P49, in ADS62P49EVM: Why there is no 50ohm impedance termination between the…
Other Parts Discussed in Thread: CDCE72010 , ADS62P49 Hi,
I have a question about the clock path between the LVCMOS driver of the CDCE72010 and the clock buffer of the ADS62P49, in ADS62P49EVM :
Why there is no 50ohm impedance termination between…