Part Number: ADS6425 Other Parts Discussed in Thread: ADS5263 Hi E2E,
Good day!
A customer of mine would like to know the theta JB of ADS6425IRGC. Also, as indicated on the datasheet theta JC is 22.1 °C/W, just want to confirm if this applies to all as…
Other Parts Discussed in Thread: ADS6425 Hi,
I'm working on a testbench board for an ADS6425 plugged to a CycloneII FPGA. The range of the input signal needs to be around 1Vpp or even less so I need to program/set the internal reference somehow to be around…
Other Parts Discussed in Thread: ADS6425 , ADS900 , ADS800 , ADS5294 , ADS5263 Hi,
I have look at the datasheet of ADS644 and ADS6425 to check if it is possible to used either in the single-input configuration. But did not find any information on single-input…
Other Parts Discussed in Thread: ADS6425 I am using the ADS6425 and I have some questions regarding the reference voltage. I am using the internal reference and it is not clear to me how to calculate the LSB size in volts. Normally I would take the reference…
Hi Richard-
We are using ads6425 for school project. the ads6425 is configured to use 2-wire and DDR for data transfer. Sadly, our code doesn't work.
Could you give some suggestion on interfacing the ads, such as DDR, and clock alignment?
Could you…
Other Parts Discussed in Thread: ADS6425ADS6425 I/O timing specifications.
The data sheet, ( http://focus.ti.com/lit/ds/symlink/ads6425.pdf ) on page 7 has a note “ Timing parameters are measured at the end of a 2 inch pcb trace (100- Ω …
Other Parts Discussed in Thread: ADS6425 After we convert the serial data output from ADS6425 to parrallel, some DataPort(1, 3, 5, ...) output square wave continously. As shown by logic analyzer in http://thumbsnap.com/VQomySEK When we input a square wave…
Thanks for your relply Xiaochen (Sean)Xu .
I have a one more question. When i use 14x serialization with ADS5295, does output data has 12 valid bit (converted data) and 2 zero padding bit like below figure? (This figure is manual of ADS6425)
Please check J6 and J8: SCLK and SDATA. These can also be used to set the output to a fixed test pattern. Refer to data sheet page 11:
www.ti.com/.../ads6425.pdf
Ken.