Part Number: ADS7028 Hi,
Some customers use ADS7028IRTE, hoping to provide related driver application routines. This chip is connected to FPGA EP4CE15F23C7N.
Please help to solve it and see if it can be provided to the customer.
Many thanks~
Part Number: ADS7028 Other Parts Discussed in Thread: ADC128S022 Hi,
ADS7028 is a relatively new product, I have customer selection, now I have some questions to know:
1. Whether ADS7028 chip is applicable to FPGA control ? If so, how do you use it? Is…
Part Number: ADS7028
Hi everyone,
Hope everyone is doing well.
I was working this ADS7028 and encountered several problems.
Most of them are cleared by reading through the following 2 posts. Now I am able to reading the ADC conversion and RMS value. …
Part Number: ADS7028 I am trying to use the ADS7028 IC to use it's special feature in outputting a 16 bit RMS reading from one of it's eight input channels. I created a circuit board for it and have it hooked up to an Adafruit ESP32 feather development…
Part Number: ADS7028 Other Parts Discussed in Thread: ADS7038 hello o am working with ads7028 adc . i need help to interface this with microcontroller using spi interface. do you have demo source code of ads7028 SPI interface. please send me if you have…
Part Number: ADS7028 Other Parts Discussed in Thread: ADS7038 Hello,
We are looking to use the ADS7028 in a new project to measure RMS.
I see that its temperature range is –40°C to +85°C and yet I see that the ADS7038 has a –40°C to +125°C.temperature…
Mouhamed,
Can you send a logic analyzer or scope shot of the communications when you do not include the delay? Include the time base in the scope shot. The device timing requirements are in section 7.6. You should not have to add 10ms in between frames…
Part Number: ADS7028 Other Parts Discussed in Thread: ADS7138 , , ADS7128 Hi Team,
Our customer is looking for an ADC that can output true RMS voltage in a similar way to the ADS7028. He needs one that has higher resolution output than the ADS7028 and is…
Part Number: ADS7028 Hello,
My customer is considering to use ADS7028 with AVDD=5V and DVDD5V. Then they have sevral questions. 1) Is any specific power-up/down sequence between the 2 rails required?
2) Is there any limitation for power ramp up speed? What…
Part Number: ADS7028 Hi,
I attempt to control ADS7028 via TMS320C2000 Experiment Kit(Piccolo F28069).
After the last discussion
( https://e2e.ti.com/support/data-converters-group/data-converters/f/data-converters-forum/1060295/ads7028-control-ads7028-via…