Koji,
It turns out that both data sheet are correct, although I understand your confusion as I also thought this was a problem. The two devices operate slightly differently. The ADS7042 has no latency. That is the conversion result for the ADC clocks…
Part Number: ADS7046 Other Parts Discussed in Thread: ADS7049-Q1 , ADS7042 Hi Team,
my customer uses ADS7046 in his project. Since we have no EVM for this device, is it possible to modify/equip one of these EVMs to the ADC:
- https://www.ti.com…
Part Number: ADS7056EVM-PDK Other Parts Discussed in Thread: ADS7056 Hi Team,
I'm currently trying to set up the ADS7056 EVM GUI, however I keep encountering a driver instillation failure when trying to install the PHI drivers (See attached image).…
Hello Cynthia :
Thank you for your kindly advice.
I'll replace the input capacitor with pF.
A question about those input capacitor that there is a document said drIving an ADC without driving OPA ( show as Fig.87 ).
https://www.ti.com/lit…
Hi Sven,
What is the noise target in uVRMS or the resolution required? We also have the ADS7056 is a 14-B 2.5MSPS ADC available on the X2QFN 1.5x1.5mm package with a thickness of 400um. It is ultra low power consumption, it consumes only 158uW when…
Hi Vijetha,
For the AMC1305 itself, there is no specific trace length requirement. Your controller is what you need to worry about - assuming you are using the AMC1035 in the uncoded bitstream mode, you have to provide a clock to both the AMC10355…
Hi I.K.,
Yes, you can most certainly use 2x ADS7054 to simultaneously sample two signals. We have a design that interleaves multiple ADS7056 devices (a faster, single-ended version of the ADS7054) to achieve a higher throughput. While not identical…
Hello Benyuan Liu,
Ideally yes, but the INAs don't typically have the bandwidth to drive precision ADC, which is why when using an INA it is recommended to incorporate an additional stage that would be able to drive the ADC or to slow sampling rate…
Dear Kim,
Thank you for your feedback. If you system does not need isolation for electrical safety reasons, like we may see with 48Vdc-fed inverters, isolation can help to improve the common mode voltage and common mode voltage transient immunity (CMTI…