Part Number: ADS7067 Other Parts Discussed in Thread: ADS7066
I plan to daisy-chain 4 ADS7067 chips on one SPI bus (shared CS and SCLK, SDO of each chip to SDI of the next) and use all 8 channels of each as digital inputs. I want CRC enabled (CRC_EN…
Part Number: ADS7067 Can you please help us achieve the maximum sample rate on this chip. tD_CKDO is defined as "Delay time: SCLK launch edge to (next) data valid on SDO: 16 ns max". When we observe the oscilloscope on SPI mode 00, we see effectively…
Part Number: ADS7067 Other Parts Discussed in Thread: TLA2518 The datasheet of the ADS7067 mentions the following: The enhanced-SPI enables the ADS7067 in achieving high throughput at lower clock speeds. And under 7.3.10.1 is mentioned: The device features…
Part Number: ADS7067 Other Parts Discussed in Thread: ADS7066 Hi there,
We are using the TI ads7067 in our custom board but a few of the channels (CH2, CH4, and CH6) are often reporting voltage under the measured value. We have an oscilloscope monitoring…
Part Number: ADS7067 In a previous post the tD_CKDO (max 16ns) spec in combination with high samplerate/SPI CLK freq was discussed. Link to post: https://e2e.ti.com/support/data-converters-group/data-converters/f/data-converters-forum/1613870/ads7067…
Part Number: ADS7067 Other Parts Discussed in Thread: ADS7066 Tool/software: Hi, we're currently looking into the ADS7067. In the Datasheet it's mentioned that you can reset it with a reset bit and also by switching AVDD off and on again. ( Content number…
Part Number: ADS7067 Other Parts Discussed in Thread: OPA325 Hi,
we use the ADS7067 in one of our applications. For the most connected analog signals we use the OPA325 as input buffer, but for some slow changing (nearly constant) signals we simply use…
Part Number: ADS7067 Tool/software: Dear Team,
Do I need to use separate LDO's for AVDD and DVDD rails.
Or Can I use a single LDO for powering the AVDD and DVDD rails.
Regards
HARI
Part Number: ADS7067 Other Parts Discussed in Thread: ADS7066 Hi,
when we apply max sampling rate (800kHz) at 50MHz SPI in on the fly mode without averaging the timings globally cannot be met formally. Do we expect too much from the component? (e.g…