Part Number: ADS7128 Tool/software: I have a few questions that are not clear to me after reading the datasheet - I do not have hardware yet to test any of this:
I would like to use the device without SCL stretching and use the CNVST bit to start the…
Part Number: ADS7128 Tool/software: Hi
Our ADS7128 is having some issues with programming.
All the registers are set as 0x4d, (Sometimes 4c) which is something that is not default of this chip, according to product datasheet.
We would like to…
Part Number: ADS7128 Tool/software: Hi,
would like to ask if there is a driver for the ADC TI ADS7128 for Linux Kernel version 6.1.34?
The environment used is BMC AST2600 with Linux Kernel version 6.1.34 to read the ADC.
Thanks!
Jeff
Part Number: ADS7128 Other Parts Discussed in Thread: ADC128S102 , TMP1075 Tool/software: I have an ADS7128 set up with 5V AVDD and 1.8V DVDD. I am seeing this unexpected issue: My 1.8V rail is at 2.3V. If I remove the ADS7128, it drops down to 1.8V.…
Part Number: ADS7128 I have the exact same question as James Long posted 11months ago, and there is no posted answer in the Forum.
Need the programming steps to set up and capture an ADC sample on the ADS7128.
I have 0.5V on CH_0 with a 3.3V reference…
Part Number: ADS7128 Tool/software: Hello.
I'm fighting with the ADS7128 I2C ADC, and I'm unable to get the RMS to work. Reading Recent value works for me (on channels 0-2 which I use). I tried to look for some example, but on github there is only …
Part Number: ADS7128 Tool/software: I am using the ADS7128 and I want be alerted when the analog threshold has been exceeded ( window comparators ) and telling the truth the device works very well in all his regards I can set the thresholds, the average…
Part Number: ADS7128 The ADS7128 data sheet says the I2C address selection resistors should be connected between the DCAP pin and ground. The schematic diagram in the BP-ADS7128 BoosterPack Plug-In Module User's Guide shows the I2C address selection resistors…