Part Number: ADS7142-Q1 Other Parts Discussed in Thread: ADS7142 , Tool/software: Dear Team TI,
I request you to please confirm whether can I refer the below application note( Monitoring NTC Thermistor Circuit With Single-Ended ADC (Rev. A) -which is…
Part Number: ADS7142-Q1 Other Parts Discussed in Thread: ADS7142 Hi team,
My customer need the ADS7142QDQCRQ1 IBIS model for the simulation, could you help to provide the model?
BR
Jingguo
Part Number: ADS7142-Q1 Tool/software: Hello,
We are using ADS7142-Q1 to detect the high threshold by configuring the device in autonomous mode with pre-alert.
Note: The alert PIN is not connected to the microcontroller.
Here is the flow:
1-Write…
Part Number: ADS7142-Q1 What could be the reason that the input collected values of the two channels of the ADS7142QDQCRQ1 chip affect each other during use? The power supply is normal. How to troubleshoot?
we use two-channel single-ended module.
Part Number: ADS7142-Q1 Hello, I'm using ADS7142Q1 convertor with thermistor as a temperature sensor. Using it in a autonomous after alert mode. Here, i'm unable to read the data from data buffer not understanding the read sequence follow by data buffer…
Part Number: ADS7142-Q1 Other Parts Discussed in Thread: ADS7142 I purchased BOOSTXL-ADS7142-Q1 and plan to test it using the Cloud GUI.
Installation was completed according to cloud instructions, but evm is not connected.
The photo below is a capture…
Part Number: ADS7142-Q1 Tool/software: Dear Team TI, I was looking forward to implement ADS7142QDQCRQ1 ADC in my design and I was going through application note of it. I could see in the formula that "100 kΩ at 25°C with a B(25/85) value of 3977" is considered…
Part Number: ADS7142-Q1 Hi, Support Team
We will use ADS7142-Q1 as below chart, about schematic have any concern?
if any suggestion, Please advise me.
Thanks,
Best regards,
Lawrence