Other Parts Discussed in Thread: ADS7223 Hi
My customer uses ADS7223 on the following condition. - Half clock - Full-differential - Mode2 (M0=0,M1=1) - SDI=GND CONVST pin receives a pulse from MCU at a intervals of 100us. CONVST pin receives a pulse…
Other Parts Discussed in Thread: ADS8363 , ADS7263 , ADS7223 Hello there.
I'd like to know if it is ok to connect the thermal pad of said ADCs to GND. I could not find any referency to this in the datasheet ( http://www.ti.com/lit/ds/sbas523b/sbas523b…
Other Parts Discussed in Thread: ADS7223 Hi,
I would like to know if I change the f(clk), how would conversion time and Acquisition time change?
If I want to Improve system accuracy, it has something to do with f(clk) ?
It would be best if there is relevant…
Hello Alex,
You are sending the sequence. This device allows for the negative pin to be set above or below ground, (-0.2V to 1.25V) as you have noted, this is primality to help with common noise. This device though is older and back at that time, the abilities…
Other Parts Discussed in Thread: ADS8363 , ADS7263 , ADS7223 , ADS7863 Hi engineers:
In ADS7263 datasheet page 17:With tACQ = 100ns, the minimum bandwidth of the driving amplifier is 19MHz for the ADS8363, 17MHz for the ADS7263, and 15MHz for the ADS7223…
Hi Victor,
See the following parts:
Part Number
Description
Resolution (Bits)
Sample Rate (max) (SPS)
# Input Channels
Multi-Channel Configuration
Input Range (Min) (V)
Input Range (Max) (V)
Interface
Integrated Features
Analog Voltage…
Hi,
The ADS8528 requires bipolar supplies as you described. Other simultaneous SAR ADC's are available; although they are not equivalent. The ADS7864 is a 500kHz, 6 channel simultaneous sampling ADC with fully differential inputs running with 5V supply…