Part Number: ADS7263 It looks like someone had already asked the question I had - is there a Verilog or VHDL model for the ADS7263 converter? This question was asked back in 2011 - just checking to see if TI or anyone else has a model for this available…
Part Number: ADS8363 I recently bought a AD8363EVM, which I'm currently trying to interface via an SPI controller (FT2232H), I noticed unfortunately
the power connector J4 isn't labelled, so I tried to deduce the pins from the schematic and PCB traces…
Part Number: ADS7263 Hi,
We are developing an application with two off ADS7263 running them in half-clock mode at 20MHz. The tolerance on the clock source is 1%, so some ADCs could see a clock frequency of 20.2MHz. Clearly this exceeds the maximum in…
Part Number: ADS7263 Hi
I have a simple question. Our customer are going to use this device at default setting of REFCM registor.
Can we leave REFIO2 floating or connect to GND as mentioned at datasheet if is at default?
Is my understanding correct…
Part Number: ADS7263 Hi
I have some question about REFIOx pin.
The register setting of the customer are below;
Config register : 0xD060
REFDAC1:0x07FF
REFDAC2:0x07FF
REFCM:0x0000
At this setting , do we need to input the some voltage to…
Part Number: DAC8814 Other Parts Discussed in Thread: ADS7263 Working on a prototype using the ttwo EVMs: ADS7263/8363EVM & DAC8814EVM, we need to prepare a custom PCB that will fit mechanically the connectors on the EVM-s - could you please share mechanical…
Other Parts Discussed in Thread: ADS7263 , OPA2365 Dears,
In the datasheet, ADS7263's application circuit is used the OPA2365. Is it specify use theOPA2365 or the OPA what need satisfies performance requirement?
If the input signal is ±10V, I want…
Hi,
Could you please help me to check the content of datasheet?
Bits[9:0] default value is 1FFh? why 1FFh = 2.5V?
For Midscale - 1LSB, the following is my equation.
AD8363 : 2.5-(5/65536) = 2.499924, same as datasheet
AD7263 : 2.5-(5/16384…
Tom,
Thanks for the response. We are using two of the ADS7263 devices in a flight control unit. We are using four channels on one and three channels on the other in pseudo-differential mode. Clock speed, mode, and temp range are as stated in the original…