Hi Idan,
The output of the AMC1100 is differential, so you want to use a differential input ADC, something like the ADS7263 as shown on the AMC1100 datasheet. Running an SPI interface over 'several feet' could be problematic, that's a bidirectional…
Other Parts Discussed in Thread: ADS7263 , ADS7945 The part ADS7945SRTER is defined up to +125 degree in most on-line shops and in your own technical specification document. Nevertheless on your web-site it is specified only up to +85. Could you please…
Priya,
I just noticed that there was new questions on this older post. In general it is best to start new thread when topic changes.
The ADS7263 is not in our HiRel portfolio, and I am not aware of any SEE data.
The TMP100 is an EP device, and currently…
Other Parts Discussed in Thread: INA118 , ADS7263 , TINA-TI Hi,
We have obtained one question from our customers. Our customers will use the INA118 as the AD Driver for the ADS7263. Although we think that the SNR will be changed in relation to cut-off…
Tom,
My customer has changed their requirements on this design, and I need your help to narrow down the right part.
Here are some recent conversations with him:
Normal
0
false
false
false
EN-US
X-NONE…
Hello Team,
Please allow me to ask you the input current to M0/M1 pins. Would the input current change by changing pull up resistor value to DVDD ?
We've monitored, Iin=300mA at 10k Ohm pull up and Iin=40mA at 100 Ohm pull up.
Best Regards,
K…
Dear TI Product Engineers,
I would like to make an additional comment. I am attaching the data sheet you provided in the past. Has anything changed since four years ago?
Junji,
SBAS952_SN201811022.pdf
Part Number: AMC1301 Other Parts Discussed in Thread: ISO122 , , RCV420 Dear Sir/Madam,
I am using single supply 4-20mA current loop receiver. I designed the circuit as per datasheet provided by TI. In that Isolation amplifier ISO 122 used as recommended…