Hello Gerald,
I have attached a PowerPoint presentation of the schematic. It is possible to drive the ADS7816 directly with the OPA340, however, it is recommended to have the RC network to mitigate 2 nd and 3 rd order effects based off of parasitic switching…
Other Parts Discussed in Thread: ADS7816 When this problem is the question to be sent to the board design maker, I understand.
But because the answer can not be obtained, I will question here.
Chip is "ADS7816". There are analog input circuit…
Other Parts Discussed in Thread: ADS8329 , ADS7816 HI.
I CONNECT ADS8329 TO LPC 1768 PINS.I CONNECT ADS8329 PIN CONVERSION TO OUTPUT GPIO
IF I CLEAR PIN FOR 200NS AND GO UP,EOC PIN OF ADS WHAT DO?
IF AFTER CONVERSION PIN GO LOW ADS8329 EOC(PIN 10) NOT GO…
Hi Tom,
Thanks for your reply! Just wondering why you suggest this option over say the AMC1100 option or Fluxgate sensor? Thank you for your reference on synchronising sigma-delta measurements.
I have come up with some potential options. I would really…
Other Parts Discussed in Thread: ADS8320 , ADS7816 , TLC4541 I have a problem with the ADS8320. This it only reads discreet values (for example 32,64,128,256,512,1024,2048, etc.) when it varies my signal of entrance. I try to use a TLC4541 and have the same…
Other Parts Discussed in Thread: ISO124 , ISO122 , ISO120 , ISO721 , ADS8326 , ADS7822 , ADS7835 , ADS7818 , ADS7816 , ADS7834 , OPA350
Dear all,
I am interested in using the ISO124 chip for protection from
switching and surge occurrences…