Part Number: ADS7842
Respected sir,
With respect to above diagram we are working on a project, which requires ADC IC.
we have few quires which we would help us proceed, the quires are as follows
1. As shown in the above picture Pin 28 is analog…
Part Number: ADS7842 Hello guys,
One of my customers is going to use ADS7842 for their new products.
They have a few questions as the follows.
Q1. Can ADS7842 be used with VDIG=3.3V, VANA=5V and VREF=5V?
Q2. When is the timing of input multiplexer…
Other Parts Discussed in Thread: ADS7842 Hi,
We are trying to use ADS7842 on a embedded force sensing system. We have 14 analog signals going into 2 channels of the ADC controlled by external 8-1 MUXs. In our program, we set the MUX first, then set…
Other Parts Discussed in Thread: ADS7842 Hi,
I am newbee to ADC process. I am trying to feed a sine wave input to ADS7842, from a function generator with a peak to peak voltage value of 5 volts. How the negative half cycle of my input will be converted…
Part Number: BOOSTXL-ADS7841-Q1 Other Parts Discussed in Thread: ADS7842
Hello all,
I am working with the BOOSTXL-ADS7841-Q1 through TM4C1294's SPI interface.
I am having a problem of getting the ADC to generate output data. I checked the timing…
Other Parts Discussed in Thread: ADS7842 hi all
I have one doubt:- I am using one ADS7842 for our application...for this reason i am using Vref=+5v,Vana=+5v, and Vdig=3.3V. should I get 0-3.3v digital swing(0=>0 and 1=>+3.3v) at the output(DB0-DB11…