Other Parts Discussed in Thread: ADS7845 , ADS7846 Hello forum:
By some remote chance, does anyone know if any Linux OS drivers exist for the TI ADS7845 5-wire resistive touch controller?
Any feedback or input is welcomed and appreciated!
Thanks again…
Other Parts Discussed in Thread: ADS7845 Hello brothers,
I want to use ADS7845 for a very low resistance five wire touch application. The screen has a resistance below 20 ohms as measured when two corners are grounded and the opposite two corners are placed…
Other Parts Discussed in Thread: ADS7845 Hello Team,
Unlike TSC2020 EVM-PDK, touch panel is not attached with ADS7845 EVM-PDK. Where would it be available??
Tosh+
Part Number: ADS7843 Other Parts Discussed in Thread: ADS7845 Hi,
I would like to ask a few questions about the ADS7843 EVB circuit:
1. Are the Analog and Digital Workspace in the EVB circuit connected to the breadboard?
2. The Analog part of the circuit…
Adrian,
We have several Touch Screen Controllers and their selection depends on not just the analog interface, but also how it is controlled. One set uses command-based technology (for example: ADS7843, ADS7845, TSC2003, or TSC2007) and a second sets uses…
Part Number: TSC2046 Other Parts Discussed in Thread: TSC2017 , ADS7845 , TSC2013-Q1
Hi all Would you mind if we ask TSC2046? Is it possible to use two coordinate detection function? Should we use TSC2017 instead of TSC2046? Or, does ADS7845 correspond for…
Part Number: ADS7845EVM-PDK Good day,
I am currently working with the ADS7845EVM 5-wire Touchscreen Controller. I am currently having problems on getting the usb device recognized on the Windows 7 (64-bit) PC.
> I tried checking all the jumpers and they…
Part Number: AM625 Hello,
I booted the rootfs.ext4 through DFU into the EMMC. After logging in, when I type the 'reboot' command in the UART terminal, the reboot worked , but ethernet is not working and the UART log shows the following.
root…
Hello Bin,
After implementing the above solution, our Ethernet continuously resets, as indicated in the following log.
root@am62xx-evm:~# reb[ 45.292173] kauditd_printk_skb: 5 callbacks suppressed
[ 45.292203] audit: type=1334 audit(1712898317…