Part Number: ADS7863A Other Parts Discussed in Thread: THS4531A , ADS7863ADS7863Aを使用して、ADCを使う場合、ADC入力信号が小さい場合に前段で差動AMPを使用します。 ADS7863Aのアナログ側は5V、デジタル側を3.3Vで使用します。 THS4531AのAMPの電源は5Vで、中点は2.5Vです。
質問1 THS4531Aの差動AMPを使用しますが、そのTHS4531AのCOM端子が入力の基準になるため、 THS4531Aの差動AMPのCOM端子をADS7863のREFIN端子に一般的には接続すべきでしょうか…
Other Parts Discussed in Thread: ADS7863 Is there anyway for this to work? All of the library's that I have tried to use (WiringPi, etc.) are configured for 4-wire SPI and not for the extra CONVST and RD wire. Is there a way to code around this, i.e.,…
Hi Peter!
No conflict really, just the wrong wording. That figure title and description should say 'recomended' timing of the RD pulse (for the original ADS7863 device). I'll get that fixed, thank you for pointing it out!
Other Parts Discussed in Thread: MSP430F2013 , ADS7863 , ADS7883 Hi, I'm trying to transfer data from the ADS7863 to the MSP430F2013 at a rate of 2MSPS. Can anyone provide any details on how to do this (code examples, pcb layouts of these connected, or…
Other Parts Discussed in Thread: ADS7863 , ADS7861 ads7863 set to mode3 m0=1 m1=0 and sdi =0 When power ON ADS7863 some times work Some times not . When ADS7863 did Not work there are no BUSY signal aways keep in low state ,and serial data A B out fix …
Part Number: ADS7863A Other Parts Discussed in Thread: ADS7863 , REF2030 Hello,
I am programming the ADS7863's DAC to adjust the REFout voltage to 1.5 V instead of the default 2.5V. Strangely, there is an oscillation on the REFout signal, see Screenshot…
Hello Ryan,
Thank you for your help.
On which clock edge will the adc start to latch the data provided by the MCU/FPGA on SDI? Also 'On SDI, the bit change occurs on each clock rising edge.' The SDI signal is an input signal for the ADS7863, I understand…
Other Parts Discussed in Thread: ADS7863 , ADS8361 , ADS7861 Hi
I'm trying to read out the ADS7863 by the McBPS of a C28346.
Now I am confused about a timing issue that is pointed out in the manual. I am referring to the data sheet of the ADS7863 from…