Part Number: ADS7863A Other Parts Discussed in Thread: ADS7948 , ADS7958 Hi exparts,
ADS7863A supports single-ended/Pseude-differential input. Can this device be used as single-ended ADC if CHAx- is connected to GND? If it is OK, what things we have…
Part Number: ADS7863A I want to convert 2 ADC readings simultaneously and read them back on a single line (OUTA on the ADS7863A). Based on the datasheet for this chip, I would like to use special mode 2 to send a single CONVST signal from my microcontroller…
Part Number: ADS7863A Hi Team,
This is FAE Jayden, my customer is using ADS7863A in their design, could you help check the schematics? Thanks.
The single-end ADC is used in their design, could you help check?
I found the thermal pad is directly…
Part Number: ADS7863A Hi Team,
We are using Part Number ADS7863ARGER. In this part number case temperature is not given so please provide case temperature of ADS7863ARGER Part.
Hello Dipen,
Thank you for your post.
Simultaneous sampling can be achieved so long as the interface inputs are shared (i.e. CONVST, RD, CLOCK, etc.).
The interface configuration will depend on the overall throughput you are aiming for and the maximum…
Part Number: ADS7863A Other Parts Discussed in Thread: ADS7863 , REF2030 Hello,
I am programming the ADS7863's DAC to adjust the REFout voltage to 1.5 V instead of the default 2.5V. Strangely, there is an oscillation on the REFout signal, see Screenshot…
Part Number: ADS7863A Other Parts Discussed in Thread: ADS7863 Hello Team,
My customer is aware of the fact, that the ads7863a replaces the older version and they use the updated version in their design. Unfortunately they can't get sufficient timing…
Part Number: ADS7863A In Mode 3 it seems like it takes 16 clock cycles before the first conversion is available at the serial outputs. Is this true?
Please respond to dcbleick@ra.rockwell.com
Other Parts Discussed in Thread: ADS7863A HI, Folks
I could not find any power sequence requirements for ADS7863A.
Does ADS7863A allows all combination of BVDD and AVDD except BVDD<(1.5 × AVDD)?