Part Number: ADS7881 Hi,
Since isolation of 2500Vrms is needed between the digital module and the analog module , we use high-speed optocouplers - ACSL-6400.
The optocoupler drive the A/D Digital inputs and the optocoupler "Output Rise Time" is 35ns…
Part Number: ADS7881 Hello,
I am interfacing ADS7881 to my FPGA. Sampling frequency = 2MHz. I am writing SDC timing commands for Timing analysis for my FPGA design and I need the Input and Output delay values for all the pins of ADS7881. I didnt find…
Other Parts Discussed in Thread: ADS7881 5226.ADS7881readproblem.pdf
We have an ADS7881 converter that cycles continuously. We build up a voltage on a capacitor, which eventually trips a comparator, which causes CONST! to go low. When BUSY goes high…
Other Parts Discussed in Thread: ADS7881 , OMAP-L138 , ADS7881EVM Hi,
ADS7881 offers parallel interface, I am wondering if it's possible to interface this data converter with OMAP-L138 EVM using UPP ? What other options are available to interface this…
Other Parts Discussed in Thread: ADS7881 Hi Tom,
I am trying to scale ADS7881 outout but I couldn't
manage to do it. I inputed 1.25 VDC to adjust R25 to mid scale
but the code axis keep moving as I move R25. However, I adjusted R25 to
set the…
Other Parts Discussed in Thread: ADS7881 The ADS7881 Specification, regarding the readout of the digitized data: The time for the DATA to be enabled onto the bus (td6) is 25ns maximum. The time for the DATA to decay from a disable (READ deasserts) is…
Other Parts Discussed in Thread: ADS7881 , AM3703 Hello-
Regarding the ADS7881 12b SAR. My cusotmer is trying to use it between a contact imagesensor and a AM3703 based SoM. His question:
"Is it safe to assume that the voltage that gets converted…
Other Parts Discussed in Thread: ADS7881 , ADS7881EVM Hi,
I have one code example which I took from the discussion page given below.
http://e2e.ti.com/support/data_converters/precision_data_converters/f/73/p/66255/289216.aspx?PageIndex=2
I don…
Other Parts Discussed in Thread: ADS7881 , ADS7881EVM Hi,
I went through the document and sample code given at the following page to interface ADS7881 with C6713 using PING PONG scheme. http://focus.ti.com/dsp/docs/litabsmultiplefilelist.tsp?sectionId…