Part Number: ADS7924 Other Parts Discussed in Thread: ADC121C027 , Hi,
We use ADS7924 and ADC121C027 on the one I2C bus, and we note that the rise time is 360ns and the high-level
hold time is 540ns. This does not meet the timing requirements of the…
Part Number: ADS7924 Tool/software: Dear TI Team
We are facing functional Test Fail , ADC values are lower for Channel-1 in IC, ADS7924, 4 Channel 12-Bit ADC with I
CH0 Behaving Abnormal
Expected Value Read : 12V Measured Value Read : below 10V…
Part Number: ADS7924 Other Parts Discussed in Thread: OPA325 , ADC121C027 Tool/software: I am using I²C at 100kHz to read ADC data. There are two ADC chips on the I²C bus: one is ADS121C, and the other is ADS7924.
I am reading data from both ADCs in…
Part Number: ADS7924 Hello,
We are using ADS7924 for data conversion. We have Voltage(0V-3.3V) and Current inputs(4mA - 20mA) given to different channels of ADS7924. I want to use Manual Scan mode in my application but I am facing issue with Manual…
Part Number: ADS7924 Dear Team,
I have some questions about ADS7924IRTER. Please help answer them as soon as possible. Thank you.
1) What is the input voltage range of CH0, CH1, CH2, and CH3 pins? Do Figure 1 and Figure 2 conflict? (As shown below…
Part Number: ADS7924 Tool/software: Hello,
Im using an arduino to communicate with the MUX (over I2C). I can set the registers, read the values... But I have very weird behaviour with the interrupt pin. It always triggers (reading INTCNTRL or Measering…
Part Number: ADS7924 Tool/software: I recently used STM32 to debug and read ADS7924. During the register reading test, I found that ADS7924 often did not respond to ACK, resulting in read and write failures.
This is my read and write process
while…
Part Number: ADS7924 Tool/software: Ref Data sheet for ADS7924 SBAS482C –JANUARY 2010–REVISED SEPTEMBER 2017
Section 6.1 - Absolute Maximum Ratings
Analog Input Voltage is quoted as:
Min (AGND-0.3)V
Max 0.3V
Please confirm this is an error…
Part Number: ADS7924 Other Parts Discussed in Thread: TLV9001 Tool/software: Hello,
I have a question regarding "Using an Operational Amplifier Between Multiplexer Output and ADC Input ".
When testing we noticed two "issues".
First of all the…