Hi Marco,
Thanks for your question! Three suggestions:
ADS112C04 : 16-bit, 4 channel, I2C interface, delta-sigma, with many features including temp sensor.
ADS1119 : 16-bit, 4 channel, I2C interface, delta-sigma, but no temp sensor.
ADS7924 : 12-bit, 4 channel…
Part Number: ADS7924 Hi,
Please let me ask the behavior when the communication error is happened.
Does ADS7924 go into unknown state if the communication error is happened during writing? Or does it reset all registers automatically?
I found following…
Part Number: ADS7924 We are using a ADS7924 in a new design. On power up, we are writing Awake Mode followed by Manual-Scan Mode. Then, every half second, we are reading six bytes of data starting at address 02h (INC bit set) and repeating Manual-Scan…
Part Number: ADS7924 Hi,
when running the SDA line @ ADS7924 with 3.3V, the chip goes onto ground and fails. Have you seen sth similar already?
Which additional details would you need?
thanks
Fred
Part Number: ADS7924 Hi Team,
If the device is configured for ALMCNT[2:0] bits of INTCONFIG(Add: 0x12) register as 111 condition for generating alarm after configured channel's conversion result exceeds the threshold limit for 7 times then what will be…
Part Number: ADS7924 Other Parts Discussed in Thread: TM4C129DNCPDT , Hello friends
I am using ads7924 in my project and i2c is the link between my tm4c129Dncpdt and ADS7924,
I have configured as per the datasheet according to me.
Now the issue is I am…
Part Number: ADS7924 Hello everyone,
I am trying to read some of the registers of my ADS7924 via I2C. I have it hooked up correctly to my F28377D controlCard 1.1. I am trying to do this via MathWorks Simulink (R2017a).
My problem is now that I do not…
Part Number: ADS7924 Other Parts Discussed in Thread: TPS24751 Hello,
I have a couple of questions on the ADS7924
can I combine AGND/DGND or do I need to keep them separate? if separate, they will be tied together locally with a 0-ohm
looks like AVDD…
Part Number: ADS7924 Hi sir :
when I used alarm interrupt,I set LLR 0x44(0.8v) , ULR 0x88(1.6V), no alarm intterrupt occurs when coversion result less than 0.8 or greater than 1.6.
But when I set LLR 0x88(1.6V ), ULR 0x44(0.8v), alarm interrupt occurs…