Part Number: ADS7951 Other Parts Discussed in Thread: ADS7128 Dear Sir, please answer
I need to measure “average voltage value” - let's call it like that, because this value cannot be called RMS.
I have signal source, figure 1. Signal…
Part Number: ADS7951 Hi Team,
In page no 43: It shows only analog ground , why is digital ground and its connection to IC DGND pin 27 and to analog ground is not addressed?
Is there a specific document for mixed signal layout for this IC other than…
Part Number: ADS7951 Dear TI specialist
can you share ADS7951 reference code,that is to say configure register code, we can more easily use the code by MCU.
thanks
Part Number: ADS7951-Q1 Other Parts Discussed in Thread: ADS7951 Hello.
There are some problems when I use read data from ADS7951 by SPI, and SPI baud rate is 500KBPS.
The application is battery management system and ADC reference is 2.5V.
Normally, all…
Part Number: ADS7951-Q1 Hello. I have raised a recent writing a while ago.
I have additional questions.
The phenomenon occasionally reads the ADC output to 5V.
Out applications are BMS(Battery Monitoring System) and system diagram is as follows.
…
Part Number: ADS7951 Other Parts Discussed in Thread: INA121 , OPA365 , OPA356 HI Ti
We have a design:
ADC_MXO connects to IN121, after amplified, output from buffer U19, then go into ADC_AINP.
The purpose is small voltage amplification (ADC Input: 1mV ~ 5V…
Part Number: ADS7951-Q1 Other Parts Discussed in Thread: ADS7951 Hello,
We are using ADS7951 device to read some analog measurements in a high power inverter application.
We are working with AUTO Mode-1 for reading the information.
Without PWM applied…
Part Number: ADS7951-Q1 Other Parts Discussed in Thread: ADS7951 , ADS1018 , HI Team,
What's the SPI pin status(the SCLK, SDI, SDO pin status specifically) for the ADS7951 when the CS is not selected(CS high)?
Are they HI-z or 0 or 1?
And also same questions…
Part Number: ADS7951-Q1 Hi Team, Our customer is requesting the leakage current of the pin numbers 1,2,29 &30 pins (Digital IOs) of ADS7951-Q1 since it is not available in the datasheet. Can you provide this information? If not, the input impedance for…