Part Number: ADS7952 Hello,
Our customer has a question for ADS7952.
When changing the channel sequence mode, for example from default Manual mode to Auto-2 mode, is a certain wait required before sending the next command?
Or is it OK to send the next…
Part Number: ADS7952-Q1 Hi,
I am using ADS7952 in manual programming mode, with analog and digital supply of 5V and separate AGND and DGND connected at one point, Vref=2.5V. In manual mode, I am not able to select range 2 (0- 2*Vref), 2.5V input to CH0…
Part Number: ADS7952 Hi Team, May I ask for help? I check datasheet of ADS7952 but I cannot find difference between ADS7952SDBT and ADS7952SBDBT. Please help confirm the difference. Thank you so much. Kind regards, Gerald
Part Number: ADS7952-Q1 HI team,
My customer is considering the front-end RC filter 47kohm & 1uF at the input pin, to have a very low cutoff frequency, any potential risk? Like lower settling time, or will it affect the measurement accuracy heavily?…
Part Number: ADS7952 Hello TI Team
1. Could you check and Explain that the IC is a monolithic integrated circuit, a hybrid integrated circuit, a multi-chip integrated circuit, or a multi-element integrated circuit?
Which of the four types is this ADS7952…
Part Number: ADS7952-Q1 Other Parts Discussed in Thread: ADS7952 Hi,
I have an ADS7952 chip with the following hardware configuration:
+VA: 5V
+VBD: 3.3V
REFP: 2.5V
Channels 4-11 in use, channels 0-3 unused
GPIO unused
When I start up, I send two configuration…
Part Number: ADS7952 Hi team,
I would like to Reset the device completely when error occurs.
Could you advise if internal registers are reset during power-down mode(PD=0)?
Or do we need to stop power supply or send reset command through SPI to reset the…
Hello Poonam,
The TLV2553 is active, here is the datasheet link - https://www.ti.com/lit/ds/symlink/tlv2553.pdf . However, we recommend using the ADS7952 as a newer alternative.
-Kyle
Part Number: ADS7952 Hi team,
Their are three ADS7952 in my customer board and there is only one SPI master.
Can our ADS7952 support SPI daisy chain as below figure? If so, is there any guidance document about it?
Is there anything needed to taken care…
Part Number: ADS7952 Hello,
Sorry if this question is quite rudimentary, but if you are using the ADS7952 and wish to use the High and Low alarm related GPIO's, what external components do you attach to these pins? The pin can go high and low, so does…