Part Number: ADS7953-Q1 Hi team,
Could you tell me the analog input maximum value? In my understanding, this max value is 5V even in both range1 and range2. Ultimately, I'd like to check if this ADC can observe 12V signal directly.
Best Regards…
Part Number: ADS7953-Q1 Other Parts Discussed in Thread: ADS7953 Hello,
I plan to use the ADS7953-Q1 with a digital I/O supply voltage of V(+VBD) = 1.8 V.
Datasheet SBAS652A (for ADS79xx-Q1, August 2014) specifies the Low logic-level input voltage VIL to…
Part Number: ADS7953-Q1 Other Parts Discussed in Thread: REF5025 , ADS7953 Hi,
In one of development project following ADC part using Qty 2 No's and individual reference generators IC's (Part No : REF5025ID) are used.
Is it okay to use single reference…
Part Number: ADS7953-Q1 Hi Expert
form below example:
ADS7953: ADS7953 SPI Auto-1 mode Configure - Data converters forum - Data converters - TI E2E support forums
the first step configure GPIO but in DS, power on step auto 1 programmable resistor is…
Part Number: ADS7953-Q1 Other Parts Discussed in Thread: ADS8168 Hi Expert
my customer have three question as below:
1. could you please share the initialize register list to me? customer want to know when device power on, which register need to set?
…
Part Number: ADS7953-Q1 Hi team,
Reviewing the ADS7953-Q1 datasheet and noticed there was no Abs. Max value for current into the device inputs. Usually there is some guidance. I've seen a lot that are usually ~2mA.
What's the abs max current limit…
Part Number: ADS7953-Q1 Hi team,
The IC runs from Vref = 2.5V reference and can sense 2 x Vref. Does the IC generate 2 x Vref internally so it can sense the full range? Or is it internally halving the input signal to accommodate a 2 x Vref range?
Just…
Part Number: ADS7953-Q1 Other Parts Discussed in Thread: TMS570LS1227 Hi,
Some of our control boards that use above mentioned part are failing configuration for Auto-1 mode. Although it works fine on the remaining boards. We are trying to figure out if…
Part Number: ADS7953-Q1 Hi team,
My customer is evaluating our ADS7953-Q1. But they will need the X-ray file of ADS7953-Q1 for internal review.
Could you kindly provide it? Thanks.
Part Number: ADS7952-Q1 Other Parts Discussed in Thread: ADS7953-Q1 , Hi Team,
ADS7952-Q1 was mass production in our customer. Due to supply issue of ADS7952-Q1, customer start use ADS7953-Q1.
Is the software of ADS7952-Q1 compatible with ADS7953-Q1? Customer…