Part Number: ADS7953-Q1 Hi team,
The IC runs from Vref = 2.5V reference and can sense 2 x Vref. Does the IC generate 2 x Vref internally so it can sense the full range? Or is it internally halving the input signal to accommodate a 2 x Vref range?
Just…
Part Number: ADS7953-Q1 Other Parts Discussed in Thread: TMS570LS1227 Hi,
Some of our control boards that use above mentioned part are failing configuration for Auto-1 mode. Although it works fine on the remaining boards. We are trying to figure out if…
Part Number: ADS7953-Q1 Hi team,
My customer is evaluating our ADS7953-Q1. But they will need the X-ray file of ADS7953-Q1 for internal review.
Could you kindly provide it? Thanks.
Part Number: ADS7952-Q1 Other Parts Discussed in Thread: ADS7953-Q1 , Hi Team,
ADS7952-Q1 was mass production in our customer. Due to supply issue of ADS7952-Q1, customer start use ADS7953-Q1.
Is the software of ADS7952-Q1 compatible with ADS7953-Q1? Customer…
Part Number: ADS7953-Q1 Other Parts Discussed in Thread: ADS7953 Hi,
There is the following chart in the ADS7953 datasheet.
question:
1, what's the test condition of Figure 10? 500ksps is the max sample rate with pwdn?
2, why the current dissipation…
Part Number: ADS7953-Q1 Hi Experts,
My customer want to add series resistors at the 4 SPI lines to reduce the noise and improve the EMI performance. For the SDO,SDI and SCLK signal, they add 51Ω at each line respectively. For CS signal, they add a ferrite…
Part Number: ADS7953-Q1 Hello,
i just confiured the SPI of the ADS7953-Q1 and I am able to read out the messages send by the SDO. I configured the ADS7953-Q1 in automode-1. But it is not possible to read the upcounting channelnrs (4 MSB).
If I watch the…
Part Number: ADS7953-Q1 Hi Experts,
My customer have some concern when using ADS7953-Q1. When the input channels Ch0-Chn are connected to 0-5V, but the power supply VA+ is absent, is there any possiblity to meet latch-up problem? If the device is latched…
Part Number: ADS7953-Q1 Hi,
in our application we might need to exceed the maximum recommended operating temperature of ADS7953-Q1 (125°C), but stay below the maximum junction temperature (150°C). Can you provide any information how it'll affect the function…
Part Number: ADS7953-Q1 Other Parts Discussed in Thread: ADS7953 NOTE: Using device ADS7953-Q1.
I have a few SPI related questions:
1. Does the ADS7953-Q1 operates in SPI Mode CPOL=0, CPHA=0? That is SDI is sampled on the rising edge, SDO is clocked out…