Other Parts Discussed in Thread: ADS8201 Hello,
I am currently debugging a board including the ADS8201 ADC.
The ADC is configured to start the conversion on /CONVST and to issue BUSY/INT. Sampling frequency is 320 Hz.
SPI SCLK is 4 MHz, here is…
Other Parts Discussed in Thread: ADS8201 Hello:
I am planning on using the ADS8201 in a new application. The software group is asking me for flow charts or algorithms to allow us to evaluate the speed and overhead limitations of running 4 ADS8201 on…
Other Parts Discussed in Thread: ADS8201 When the input voltage is crossing the 2,5V with a sine wave signal, see the picture below. If the sine wave is all the time below or above the 2,5V, there is no spikes visible. Is the problem in the communication…
Other Parts Discussed in Thread: ADS8201 Hello,
We
are currently using the new ADS8201 ADC.
The issue is that we can't find information on how to
properly use the ADS8201 in Auto Trigger, Auto Channel modes with the
FIFO enable.We can Initialize…
Jose,
Hang in there, we'll get it figured out.
It appears as though you are communicating correctly. Have you tried reading the 0 channel without writing anything to the part? The default mode is 2, and the default channel configuration is 0. It…
Hi,
How are you?
our system engineer mentioned since our device is not used for very low frequency signal
and he recommended the following:
=======================
ADS8201 could be a good one for 4Hz to 8K signals.
also why you look at aFE5801…
Hi Wenting,
Most of the precision ADC portfolio is based on higher speed products using an SPI interface. Such devices include TLV2544 family, the TLC2574 family and the ADS8201. You could also look into the ADS7142 which is an I2C interface. Another…
Hi Shawn,
Unforturnately, we do not have an ADS8201 evaluation board released. I am out of the office this week; however, If you wish to provide your contact information directly via email at l-chioye@ti.com
Best,
Luis