Hi there.
I am having problems with the ADS823 converter. I used the recommended circuit shown in the Fig. 2. of the datasheet but I am only getting one bit conversion output. I mean, every out pin gives the same output voltage. When the input signal…
Hellow, I am having problems with ADS823 converter. I am using a FPGA to capture the digital data output from a A/D converter. I did the same circuit as shown in Figure 2 datasheet. I put the input signal at ground, then the signal input of the A / D is…
Hi Jim,
After replaced OPA698 with LMH6702, there's no improvement. in ADS10321 datasheet page 14, "The use of an internal sample-and-hold amplifier (SHA) enables sustained dynamic performance for signals of input frequency beyond the clock rate…