Part Number: ADS8317 Other Parts Discussed in Thread: ADS7066 Hello,
Do we have any demo code or example code we can share for setting up the ADS8317? My customer would also be interested in help with implementing filters on the incoming data if we have…
Part Number: ADS8317 Other Parts Discussed in Thread: ADS8863 Hi Team,
My customer is considering ADS8317 and he has one question.
He wants to use it with Vdd = 5.0V±5% and Vref = 2.5V.
Datasheet says recommended Vref range is 0.5V~Vdd/2 when VDD…
Hi Daniel,
Thanks for your question! Looking around, perhaps the ADS8317 would be a good fit. Let me know if it doesn’t meet your needs and I can offer some other alternatives as well.
Best regards,
Samiha
Part Number: ADS8317 Hello E2E, I have the same case as the URL below at now. e2e.ti.com/.../649030 The incidence is about 100 / 20k units in a year.
If you know the cause, please let me know it.
Regards, ACGUY
Part Number: ADS8317 Other Parts Discussed in Thread: THS4551 , THS4521 Hi,
I would like to use THS 4131 for the input amplifier of the ADS8317.
Is there a reference design for the differential input of the ADS8317?
Is there any op amp recommended other…
Part Number: ADS8317 Hi,
I have a customer using ADS8317 in their products. Waveform jumps when output code is near zero.
ADS8317 Data Sheet P.16 THEORY OF OPERATION I found the following description.
Differential linearity for the ADS8317 is factory…
Other Parts Discussed in Thread: OPA2365 , ADS8317 My ADS8317-based project is almost done, thanks also to the help I got from here. Everything is already working well, the values I get are generally sensible, but I noticed one (final?) problem:
When I…
Other Parts Discussed in Thread: ADS8317 , CSD I understand that the ADS8317 uses falling edges of DCLOCK to set up data, so that data should be sampled on the rising edges of DCLOCK.
The timing diagram looks like it should be OK to use either SPI mode…
Other Parts Discussed in Thread: OPA2376
The datasheet of this part shows that it has protection diodes on the signal inputs, which have a VF of 0.35V. The maximum ratings say "Input current to any pin except supply: -20mA to 20mA" It also says "Analog…
Hello,
I use the following schematic and SPI code below :
The voltage reference used is +3.00V
I consider the following calculation : V+ = Vpress = ( ADC / 32768 ) x Vref
I think i could have made a mistake in the code source because i can't get a correct…