Part Number: ADS8319 I had a question about the ADS8319 There is an ADS8319 we currently use in our product I am interested in the ADS8319B as an alternative
Are these the same die and just screened differently or are they two different die?
Part Number: ADS8319 Hello Team,
does the ADS8319IBDRCR has a thermal pad below?
The datasheet is not clear on that:
Page 39 - 3D modelling has the thermal pad.
Page 40 - shows the thermal pad.
Page 41 - contradict all, and says - No exposed thermal…
Other Parts Discussed in Thread: ADS8319 Hi there,
I've recently done a design using the ADS8319 in 3-wire CS without busy indicator mode and am having troubles interfacing with it. My circuit looks like this:
IN+ connects to a buffer which is biased…
Hi Ben Collier,
Below is the block diagram of current sampling circuits, as the power rail of ADS8319 is higher than F2806x, customer wants to use R1 and R2 divided resistors to decrease the voltage range within 3.3V
As there need to impedance balancing…
Part Number: ADS8319 Hi all
My customer is using the ADS8319 and he has below question.
Please comment and clarify.
Thank you and best regards
Ueli
----------------------------------------
I have some difficulties in correlating the information from Table…
Part Number: ADS8319 Hi all
My customer is using the ADS8319 at 30ksps and he has this quesiton:
On page 11 of the Datasheet there are ENOB-plots vs. various parameters, all given at fs=500ksps.
Do these numbers change when going to 30ksps ?
And if yes…
Part Number: ADS8319 Other Parts Discussed in Thread: ADS8864 Dear all,
I would like to ask about Daisy-Chain option in ADS8319.
For the ADS8319, how many channels can be sampled simultaneously using the Daisy-Chain Option?
I need to know the answers…
Part Number: ADS8319 Dear all,
I would like to ask following questions about datasheet.
1.According to Fearture on page 1 of the data sheet, the input voltage range is indicated as Single-Ended Input Range: 0 V to VREF.
Is it safe to assume that this…
Part Number: ADS8319 Dear Team,
My customer is considering the ADS8319 for a new design.
1. Is there any power sequencing requirement for the device ?
2. For power saving, is it possible to supply one of the supply types without supplying the other for…