Part Number: ADS8320 I'm looking to use the ADS8320SKGD1 (die) 16-bit A-to-D converter in an MCM for an application requiring TID (total ionizing dose) radiation performance of 50 krad(Si). I understand that the ADS8320 is NOT an inherently radiation…
Part Number: ADS8320 Tool/software: Hi
I am sorry for this petty question but i did not find a formal answer in ADS8320 documentation : is DOUT output type format tri-state or CMOS ?
Thanks for help
Olivier
Part Number: ADS8320 Other Parts Discussed in Thread: ADS8867 Tool/software: I have few questions in regards to the fabrication history of the ADS8320E/250.
I am seeking a replacement for the ADS8320E from Burr Brown Coporation (Cage code 13919)
From…
Part Number: ADS8320 Hello,
I have some oveshoot on the SPI signals going to the device and i was wondering if the overshoot and undershoot pulses were shoot enough that it wouldn't cause reliability issues.
The overshoot goes up to 8V and is above…
Part Number: ADS8320-HT Other Parts Discussed in Thread: ADS8320 The ADS8320SHKQ DAC only specifies Voh = 2.1 V minimum with 2.7 VDC supply and does not specify value with 3.3 V supply. In my design I am using 3.3V supply and this doesn't give a very…
Part Number: ADS8320 Other Parts Discussed in Thread: SN74LVC4245A Hi,
I have some troubles with the component ADS8320. I develop an electronic card to take measurements. In this card there are 2 ADS8320. Their input are different but their output are…
Part Number: ADS8320 Other Parts Discussed in Thread: PSIEVM , LMP7716 , OPA354 Hi, All:
We are planning to use ADS8320 in our project, and we bought an ADS8320EVM and are evaluating the baisc features.
Now we met an issue of SNR.
We tested your…
Part Number: ADS8320-HT
Hi,
According to customer, the bond pad coordinates do not match in the picture in the datasheet.
https://www.ti.com/lit/ds/symlink/ads8320-ht.pdf?ts=1649699327872&ref_url=https%253A%252F%252Fwww.ti.com%252Fproduct%252FADS8320…
Part Number: ADS8320 hi dear supporting team,
customer is using ADS8320 with below sch(share the same circuit with AD7683). They found there is close to 1V glitch at Vin pin, which has same cycle with Cs signal. the input is disconnect with previous…
Part Number: ADS8320
Hi team!
I have a project use ADS8320.schematic as show below
After power up and do not any communication and the current consumes about 54uA. After powering off and on again, the current consumption is not fixed at 54uA or…