Other Parts Discussed in Thread: ADS8326 Hi All,
I am looking for the fdclock specification for this part when operating at Vdd=3.3V. The data sheet lists fdclock at 2.7V (4.8MHz) and 5.0V (6MHz), but not at 3.3V. What is the fdclock maximum specification…
Other Parts Discussed in Thread: ADS8326 , ADS7924 Dear TI,
I need to know if it's possible to use the ADS8326 with the SSI interface instead than SPI. If yes how?
Best
M
Part Number: ADCPRO Other Parts Discussed in Thread: ADS8326 , ADS8326EVM-PDK Hi,
We tried using the ADCpro to test an ADS8326EVM.
The EVM motherboard came up in the device manager as "unknown device" and would not allow any drivers to be installed. I…
Other Parts Discussed in Thread: TXB0104 , ADS8326 , LM358 , REF5040 , OPA365 OBJECTIVE
To measure DC voltage in a flexible, automated test rig for high voltage power supplies, with the system based on a Raspberry Pi or similar inexpensive single-board computer…
Other Parts Discussed in Thread: ADS8326 , TXB0106 , SN74LVC1G125 , SN74LVC2T45 Hello-
For the ADS8326 running off 5V, what is the maximum low outpout voltage for Dout at 2mA load?
For the ADS8326 running off 5V, what is the minimum high outpout voltage for…
Other Parts Discussed in Thread: ADS8326 , ADS8866 I need to make a simple voltage measurement device to measure up to 5v positive only but am unsure what ADC I should use.
I need it to be accurate to at least 1mv and a 16bit resolution would be nice, the…
Other Parts Discussed in Thread: ADS8326 , TINA-TI , REF5030 Hi,
Is there a model of ADS8326 on tina-ti Spice ? I don't found it on the database of http://focus.ti.com/adc/docs/midlevel.tsp?contentId=31690 .
Thank you for taking time.
Steven
Part Number: TLV07 Other Parts Discussed in Thread: INA818 , OPA320 , OPA325 , ADS8326 We are trying to implement instrumentation amplifier using tlv07 opamp to amplify 10mV signal 500 times. The circuit is something like this(the voltage source provides…
Jack Summers11 said: To do this, I think I need to set up the clock and CS pins as pwm signals and trigger the SSIDataGet command off of the CS timer. When the TM4C123 SPI module is the SPI master, then the SPI module needs to generate the clock by cal…
Other Parts Discussed in Thread: ADS8326 Dear All:
I have use ADS8326 to convert a voltage:0--5V;
My Program is:
////////////////////////////////////////
uint AD_Convert(void) { uint i; uint result; CS=1; delay(1,1); CS=0; delay(1,1);
for(i=0;i…