Other Parts Discussed in Thread: ADS8332 Hallo erverybody,
I am currently working in an analog-to-digital converter ADS8332 and have problems with the use of this IC. This IC communicates with the microcontroller over the SPI. I'm a novice in this area…
Other Parts Discussed in Thread: TMS320F28335 , ADS8332 , DAC8760 I am planning to use the DAC8760 EVM and ADS8332 EVM at the same time as slaves of DSP TMS320F28335, ADC is in a 16bit SPI communication and is working properly using the code example here…
Other Parts Discussed in Thread: ADS8332 I am having a problem during trying an example downloaded here in your website for the Interfacing of the ADS8332 to DSP F28335, so I am requestiong for someone's help for just giving some example codes in writing…
Other Parts Discussed in Thread: ADS8332 Hi,
I'm trying to convert a 50uV differential signal (output from a sensor). I'm looking into ADS8332. Accuracy at this point is very important. Pls help to comment if i look into the correct IC or is there a better…
As we are using ASD8332 ADC we got a problem regarding mode of selection. In auto mode we are able to read the data from channel 1 to 8 but while configuring in manual mode we unable to get the data of the desired channel.also in this mode we are getting…
Other Parts Discussed in Thread: ADS8332 Hi:
I can't switch ADS8332 mode by writing CFR. When I write CFR and read back, the CFR seems not write into ADS8332, when I read back, it only shows default value. Can Someone help to check timing or what I should…
Other Parts Discussed in Thread: ADS8332 Hello,
I need a bit of a help with ADS8332. It is set to 0x7FD (no AUTO_CHANNEL, no TAGS) and communicates with processor (ATmega128, 20 MHz) just fine. Some time ago I've noticed that sometimes the chip suddenly…
Other Parts Discussed in Thread: ADS8332 Hi:
I'm using ADS8332 with default configuration mode (all CFR is default value "$FFF). It implies auto channel selected, manual trigger, tag bit output enabled, Nap/Deep power down disabled. Only one ADC8332 is…
Other Parts Discussed in Thread: ADS8332 Hi, I am a newbie in using ADC data converters.
I used ADS8332 and interfaced it with bus pirate. On initialization I wrote [0xe4,0xfd]. Then upon reading the bytes on the CFR register I always get 0xffff on the…