Part Number: ADS8343 hi team:
regarding the ADS8343 device, do we have a reference code for primary inspection?
as the below SCH, if we do not connect the busy PIN to MCU , is that okay to follow up the timing with SPI without indication from busy signal…
Part Number: ADS8343 Hi,
Who can help with identification of microchip`s marking?
Part numbers are ADS8343E and ADS8343EB
So, if base on packaging part marking lookup, model ADS8343EB must have this part number: ADS B 8343E But in facts i have this one: …
Part Number: ADS8343 Hello,
A customer is redesigning a board with the ADS8343 on it. They had the below questions:
Do we have an example schematics (EVM or reference design) for this device?
What is the input impedance of the analog input, or what is…
Other Parts Discussed in Thread: ADS8343 Hello,
I'm trying to decide which configuration of the ADS8343 will result in less noise on the device. On my layout, I currently am only using one of the input CHX channels (CH0), while the others are left floating…
Other Parts Discussed in Thread: ADS8343 We are having trouble getting the ADS8343 into internal clock mode. We are setting PD1=1 and PD0=0 (selects internal clock mode) but from monitoring the busy line it appears to actually be in the external clock mode…
Other Parts Discussed in Thread: ADS8343 Hi,
I am trying to use an ADS8343 ADC. I am going through the datasheet to figure out if this does what I need. I am looking for something that measure voltages between -2.5 and +2.5.
So far I think this chip will…
Part Number: ADS7953 Other Parts Discussed in Thread: ADS8343 , , ADS1112 , ADS1118 , ADS1115 hello
we have a new project that need 20channel ADC,because this project need modify on the exisiting project and ,that project has used ADS7953 which is 16 channel…
Hi Jishnu,
No, you can not change the BW of internal LPF. Also, when you use this ADC to measure a high frequency signal (e.g. 15kHz), your signal will be attenuated and distorted by the LPF. There are two possible solutions:
1. Use an ADC with integrated…
Hi Shrikant,
The first parts that come to mind are those from the ADS834x family. The ADS8341 and ADS8343 are quad 16-bit parts while the ADS8344 and ADS8345 are octal devices.