Other Parts Discussed in Thread: ADS8361 , TMS320F2812 I'm still trying to interface an ADS8361 with an F28335. It looks like I have some timing issues when reading the data using the McBSP. I tried to follow the code and the schematics included in this…
Other Parts Discussed in Thread: ADS8361 I'm using an F28335 micro-controller to implement a PID controller. The internal ADC has a limited resolution (12-bits) so I opted for an external 16-bit ADC, the ADS8361. The ADC data sheet shows a 4-channel…
Other Parts Discussed in Thread: ADS8361 , CONTROLSUITE In regards to internal ADC12 to RAM via DMA, is there is demo code to try out?
In regards to external ADC16 (ADS8361) to RAM via DMA using McBSP module, how the DMA is configured for continuous sampling…
Hi Tom,
thank you for coming back. However in the meantime many principles could be understood .
Therefore to conclude this thread I would like to post the following:
In the scope image below, input to the ADS8361 and output from the DAC8554 can be seen…
Other Parts Discussed in Thread: ADS8361 If I give a 3.3V supply to BVDD pin and a +5V supply to AVDD pin of ADS8361, will I get a 3.3V high and 0V low digital outputs at the the digital out pins???
When I saw the datasheet, it is written digital out will…
Other Parts Discussed in Thread: ADS8361 Hi all,
i have a problem interfacing an ADS8361 with a 32-Bit-Microcontroller. I am using an STM32F4 eval-Bord.
I want to use mode IV, i followed an example, what i found in your website. I use the logic analyser…
Other Parts Discussed in Thread: ADS8361 Hi, I'm planning to use ADS8361 for a 4 channel FSK-FH decoder, using 6418EVM, 5-6k interface board and ADS8361EVM .
I want to use mode IV operation of ADS8361 , and have the 4 channels 16 bit samples written by…
Other Parts Discussed in Thread: ADS8361 , TMS320C6748 Hi.
I'm using TMS320C6748_GEL_BSL_Files in EVMC6748 to connect with ads8361 and c6748 by using McBSP & EDMA.
I'm searching for McBSP, EDMA BSL for c6748 (non-bios),
but I can't find McBSP &…
Other Parts Discussed in Thread: TMS320C6746 , ADS8361 Hello,
I couldn't find example code for McBSP interface to bring up ADS8361 and TMS320C6746.
I only found below article in this link http://www.ti.com/lit/an/slyt053/slyt053.pdf as below, but the…
Hi Serkan,
As you told, unfortunately, on the datasheet you can only read informations about the 20-bit reading way.
You can see how I did looking at a zipped file I posted some time ago in this discussion (in which you can find some pictures took from…