Part Number: ADS8363 Other Parts Discussed in Thread: ADS9324 Hi team,
In order to synchronize the conversion and reading of 2 ADS8363, I was wondering if ADS8363 family supports SPI Daisy-Chain configuration so they can be seen as 1 peripheral from…
Part Number: ADS8363
Tool/software:
Dear Team,
We are using ADS8363 for our application.In our schematic we didn't connect the M0 and M1(NC) Pin and our operating mode is Half clock mode(Mode-1),this configuration is correct or not?.
Is there…
Part Number: ADS8363 Tool/software: Hi Sir,
In the datasheet of the part ADS8363SRHBT, it is not mentioned with the connection of Thermal pad(Exposed pad). Please confirm whether thermal pad is required to connect either to DGND or AGND.
with regards…
Part Number: ADS8363 Other Parts Discussed in Thread: AMC3330 , ADS1119 , ADS1120 , ADS112C04 , Hi team,
My customer is designing an insulation resistance measurement circuit based on the TIDA‑010232 reference design. They would like to route the AMC3330…
Part Number: ADS8363 Tool/software: Greetings from datapatterns!
Sir,
We are planning to use your product ADS8363 for our application, Kindly confirm whether it may works when CMA and CMB pins were kept floating.
with regards
Tanniya S
System…
Part Number: ADS8363 Tool/software: Hi, I am looking to use the ADS8363 REFIO output as an excitation source (with an external buffer to increase output current) for a strain gauge sensor in a bridge. I am looking to make an accurate noise simulation…
Part Number: ADS8363 Hello,TI data converter experts:
We are using ADS8363 for two channel simultaneous sample.We use a FPGA to drive ADS8363,the problem we are facing is that sometimes when powering up ADS8363 load error and get wrong data,typically…
Part Number: ADS8363 Hello,
I am using this ADC on my board with the device configured to use only one shared reference (REFIO1) for both internal ADCs on the chip. The resulting data was extremely noisy to the point that we were only able to use 12…
Part Number: ADS8363
Hello team,
If my customer wants to use ADS8363 with 0-5V SE input,
CMA pin should be connected REFIO or 2.5V. Is this right?
Do they need to connect (-)input with REFIO or 2.5V?
Or both connections must be required?
Best…
Part Number: ADS8363 Hi team,
My customer has a question regarding the full-clock mode of ADS8683.
When the IC /CS signal is enabled, there is a rising edge of CONVST, but SDI and RD seem to be ignored and take no action according to the pin function…