Part Number: ADS8363 Other Parts Discussed in Thread: INA250 Hello, could you guide me in the use of the M0, M1 and CONVST pins?
I have a differential input and three pseudo-differential inputs that I need to sample. Given this how should I configure…
Part Number: ADS8363 Other Parts Discussed in Thread: ADS5263 , ADS8694 , ADS9224R Hi there:
We'd like to find an solution with 18-bit SAR ADC (4XADC), 1MSPS criteria.
The most closest us ADS8363, but it only has 16-bit.
Do we have 18-bit one? or…
Part Number: ADS8363 Hi,
On the ADS8363, my customer is seeing the codes for signals on the negative side of the 2.5V bias go near saturation even though the input signal is nowhere near saturation level. This is at high temp (> 40 deg C) when powered…
Part Number: ADS8363 Hi,
It is described that NMC of the ADS8363 is 15 bit or 16 bit as below.
How do the ADS8363 work as NMC 16 bit?
Best Regards,
Kuramochi
Part Number: ADS8363 Hi,
I am taking 2048 samples from a ADS8363 using SPI at a frequency of 10Mhz. When I take the first reading the first value of the 2048 samples is always pegged high, the rest of the values are normal. If I take another reading…
Part Number: ADS8363 Other Parts Discussed in Thread: ADS8353 , ADS8860 , ADS8332 I had some initial problems with the ADS8363 which were related to the timing between the Rd pulse and the clock pulse. I changed that timing which kind of solved the problem…
Part Number: ADS8363 Other Parts Discussed in Thread: ADS8361 , TMS320F28377D The ADS8363 Dual SAR ADC has a serial interface with a single CLK, single SDI, but dual SDO, one for each SAR ADC. The best way to interface this to a uC is not obvious, including…
Part Number: ADS8363
The input signal can be btw 0 and 5V. If the signal is below 2.5V it should be a signed binary number. If the signal is above 2.5V it is a positive number. Will hardwiring 2.5V to pin 31 (CMA) provide what the pseudo-differential…
Hello Linh,
I have to apologize, I made a mistake when looking for the ibis models, the device with the ibis model is ADS786 3 not the ADS786 1 . I am sorry for the confusion on my part.
ADS7863 is similar to the ADS7861, but it has additional features…
Part Number: ADS8363 I am using the ADS8363 with an STM32F407 processor and interfacing to the ADS8363 with the processor’s SPI interface. I have not figured out a way to send twenty clock pulses to the ADS8363, instead I am sending three eight bit bytes…