Part Number: ADS8548 Hi team,
I want to increase the sampling rate of ADS8548, which is mainly used for the analog signal sampling of sine-cosine encoders, to achieve a sampling frequency of over 300K. Currently, I am encountering some issues, please…
Part Number: ADS8548 Other Parts Discussed in Thread: SN74AHC1G04 Tool/software: I have a question about ADS8548.
I produce some ads8548 boards. The refio pin of some boards is 4.966V, and some are normal(2.5V). why?
Part Number: ADS8548 Other Parts Discussed in Thread: ADS8684 Tool/software: Hi team my customer wants to know how to calculate the conversion time since sampling the analog data and then output to MCU. do u have any advise?
Part Number: TMS320F28379D Other Parts Discussed in Thread: ADS8548 Hello,
I was thinking about interfacing the TM320F28379D's EMIF with the ADS8548. However, I think there would be an issue meeting the tHDO and tDTRI requirement because the Data changes…
Cynthia,
Also is there any information for Radiation level or some tests done for ADS8548 that we can have those documents?
Any documentations or extra paperwork regarding radiation test will be helpful and usable!
Also if TI can provide useful…
Part Number: ADS8548 Hi All,
I have a question about ADS8548
I confirmed that 5V was output from the REFIO pin. I think that 2.5V to 3V is output from the REFIO.
Do you know the cause of 5V output from REFIO?
Best Regards, Ishiwata
Part Number: ADS8548 Hi,
When ADS8548 is used, its HVDD and HVSS are connected to 5V and 0V respectively, and the input analog signal is ensured to be within 0V~5V (AVDD and DVDD are connected to 5V and 3.3v respectively),
I would like to ask if there…
Part Number: ADS8548 Hi team,
I wonder is this device able to read data for a certain channel at one time instead of reading all the 8 channels? And how?
Thank you very much!
George
Part Number: ADS8548 Hi Team,
My customer feedback that why did the Internal Reference voltage change from default 2.5V to 1.031V after ADS8548 was running 2 hour?
They used ADS8548 default Internal Reference 2.5V. ADS8548 is controlled by FPGA…
Part Number: ADS8548 Other Parts Discussed in Thread: ADS8568EVM-PDK I am using the ADS8548SRGC ADC and the thermal pad on the device has been connected to the Ground plane using multiple Via’s for better heat dissipation.
Can the thermal pad be connected…