Part Number: ADS8556 Hi team,
I help my customer to ask a question.
“
I want to emulate ADS8556 in pspice but I don t know how to use these models.
Directly output without an power supply?
What is difference for DIN_5 and DIN_3?
What means about…
Hi Jimmy,
Thanks for the clarification.
The team has not seen this before and is not exactly sure what the issue could be. There's a possibility there is a power supply sequencing or specification problem but we can't see this. As a result, we need some…
Part Number: ADS8556 Hi team,
My customer is splitting the input signal into 3 and putting them to CONVST_A,B,C. This is for HW mode. Now, my customer is wondering if they can use this configuration for SW too. Can they use same configuration for SW mode…
Part Number: ADS8556 We are using ADS 8556 in single ended sensing mode. output of ADC is connected serially ( SPI ) to Microcontroller.
1) we are giving input -10 to 10 V to channel . what we should expect at output whether it should show Count from…
Part Number: ADS8556 Hi team,
Regarding to this thread,
https://e2e.ti.com/support/data-converters-group/data-converters/f/data-converters-forum/1091657/ads8556-voltage-value-on-refc-pin-and-power-sequencing-of-ads8556?tisearch=e2e-sitesearch&keymatch…
Other Parts Discussed in Thread: ADS8556 Dears,
I use DSP F28335 to expand ADS8556. When sampling, the input signal will produce many spikes, which will affect the sampling; In addition, signals between channels will also affect each other. For example…
Part Number: ADS8556
First of all, hello, I am using the ADS8556 ADC card. In the project I will do with this card, I use hardware mode with serial interface, so I need to communicate with SPI. Can you help me on this issue?
Part Number: ADS8556 Hi Team,
My customer is considering ADS8556 and he has following 2 questions. Could you kindly help?
1. From following block diagram, REFC_A, B, C seems connecting with output of a buffer, customer wants to know what voltage level…
Part Number: ADS8556 Other Parts Discussed in Thread: OPA171 Hi,
We are using two ADS8556 in serial interface (not in daisy chain). I have following questions on front end and circuit configuration:
For front end where signal frequency is up to 4.4KHz…
Part Number: ADS8556 Hello, I am performing Signal Integrity analysis using ADS8556IPMR IBIS model available on following link : www.ti.com/.../sbam011
with DIO_3 buffer model as an input buffer, I am getting 3.3V at an input of this Buffer as expected. But…