Hi Yolanda,
Thank you for the detailed response.
May I send you more details via a personal message regarding the application?
I will review the rest of the documents provided and might ask a question or two regarding the calculations.
Thank you for all…
Part Number: ADS8568 Hi,
regarding to figure 45 of the ADS8568 datasheet i want to ask if anyone can please recommend me suitable voltage/potential transformers and current transformers for a simultaneous acquisition with the ads8568 of voltage and current…
Part Number: ADS8568
Tool/software:
Good day everyone,
I plan to use 3 ADS8568 adcs connected in a daisy chain configuration with a series output, configured via hardware mode and each with their own internal clock.
The input voltage from the driving…
Hello Ryan,
Thank you very much for your reply and I'm sorry to be late my response.
I asked them to turn on after going down less than 0.3V. They will add any delay circuit for re-powering up.
Thank you again and best regards, Kazuya.
Part Number: ADS8568 Tool/software: If we start pulsing /RD after the BUSY goes low, but /CS goes low a little later, after some /RD pulses have already been made (let's say 2). Will the data on the parallel bus for the 3rd /RD pulse (first with /CS…
Part Number: ADS8568 We have a design with 10 ADS8568 boards in a rack with an FPGA reading the SPI buses on the backplane. We have some amount of ringing on all of the signals to/from the ADCs and we believe that we are getting occasional spikes on the…
Part Number: ADS8568 Other Parts Discussed in Thread: ADS8528 Hi,
My customer wants to know the specific parameters of the ADS8568:
1. The ADS85x8 series is an 8-channel ADC. What does it mean in the specification that the maximum data rate per channel…
Part Number: ADS8568 Hello, We use the ADS8568 in one of our designs to monitor 60 Hz signal quality. We have a signal stability problem at low temperature in our qualification tests. The problem occurs on at least ONE channel of SOME systems only. It is…