Part Number: ADS8568
Hi Team,
We received this inquiry from our customer.
In the datasheet for the ADS8568 it is stated that the minimum voltage levels with which the device will function for HVDD and HVSS are +5V and -5V respectively. However,…
Part Number: ADS8568 Dear data converter experts,
I have a question about gain error and gain error drift when external input to REFAP,REFBP,REFCP,REFDP.
I would eliminate gain error (0.5%) and gain error drift (10ppm/°C) from internal buffer. …
Part Number: ADS8568 Other Parts Discussed in Thread: ADS8556 , We have an ADS8556 in an old design, connected in Hardware Mode and not updating configuration register. Parallel data transfer. We have made another design using ADS8568, connected in Hardware…
Part Number: ADS8568 Hi Team,
The customer is having issues with the ADC SPI communication. Kindly refer to the information below:
I can read te data but from time to time the ADC « fails » to convert data.
I follow the datasheet and code a SPI…
Part Number: ADS8568 Other Parts Discussed in Thread: ADS8588H I'm having trouble finding part ADS8568SRGCT in the Channel.
Is there a different part that is comparable that is more readily available, please?
Part Number: ADS8568 Hi,
There are a couple of questions and issue.
1. Does t(ACQ) mean charging time of internal capacitor or acquisition time of conversion data from ADC to MCU?
2. If it's charging time, is internal capacitor charged in t(CONV…
Part Number: ADS8568 The voltage range of MicPhone signal is usually between 0~3.3V. Can ADS8568 accept this unipolar analog input signal?So, can HVDD connect to 3.3V and HVSS connect to Ground?
Hi Ray Ni,
I don't believe that the UPP interface is the correct connection for the ADS8568. The UPP was design for connection to a synchronous interface that is running continuously. It is also unidirectional with a channel in and a channel out. The…