I have not received your response for almost one month, this thread will be closed. You can post a new query if you still have any questions. Thanks.
Regards,
Dale
Part Number: ADS8584S Other Parts Discussed in Thread: ADS8588S , ADS131M08 The data sheet states that the power consumption at 330 kSPS is 54.mW. How about the power consumption at lower sampling frequencies say 20kSPS? I'd assume it should be less. Where…
Hi David,
Thanks for your response. I proposed to postpone the meeting to 10am today but did not get response. Please check with Yaron if you still want to discuss directly.
I summarized the issues your have:
a. High level of BUSY is only 1.7V which is…
Part Number: ADS8584S Hi,
Im tring to make the ADS8584S work with a SAMD51 however the output data seems to be wrong.
AIN_1P is connected to a static 2V output.
AI1N_1GND is connected to GND.
The rest of the ADC Input arent connected.
PAR/SER/BYTE SEL…
Part Number: ADS8584S Hi team,
a customer is currently using the ADS8584. we are aware that it has a max throughput of 330ksps.
however, they might need to sample the signal closer to 0.5Mbps and waive the simultaneous sampling function.
they haven't…
Part Number: ADS8584S Hi Ti team, I am (from SFO Technologies) using adc part no: ADS8584SIPMR in serial mode with 20MHz SCLK, but I am not able to receive valid data (it is continuously zero "0" is coming). Can you please provide a sample code in c/c…
Hi Matt,
The digital filter on delta-sigma ADCs require time to settle after a resynchronization event occurs, and they do not have a dedicated CONVST Start pin. Many SAR ADCs have a dedicated CONVST Start pin which can be used to synchronize with an external…
Part Number: ADS8584S Other Parts Discussed in Thread: TLV759P , , LP38798 Hi Team,
ADS8584S is used in our application, for the power supply for AVDD, can TLV759P( http://www.ti.com/product/TLV759P )(High noise, low PSRR) meet the requirements of ADS8584S…
Part Number: ADS8584S I am using the ADS8584S in a high speed analog acquisition system.
The ADS8584S is set up with CONSTA and CONSTB tied together, CS and RD tied together, 5V power, parallel data mode and +5 and -5 input scale.
The ADS8584S works…
Part Number: ADS8584S Hi ,
Please find the attached block diagram. I am planning to use ADS8584S for measuring current consumed by our DSP at its different operating modes. Current varies from 10uA to 100mA.Need some clarifications regarding the signal…