Part Number: ADS8588H Hi,
Is there an IBIS model available for the ADS8588HIPMR? Hoping to add the digital side of the ADC to my signal integrity analysis. The IBIS model is not available in the standard Design tools & simulation tab of the product…
Part Number: ADS8588H Other Parts Discussed in Thread: TINA-TI Dear Sirs
I am looking for a Pspice Model for ADS8588H if possible.
Thanks a lot and Regards
Sal
Part Number: ADS8588H Tool/software: Hi,
A customer is designing a measurement circuit for grid infrastructure using ADS8588H.
Q1. Is there a way to diagnose ADS8588H failure? If registers etc. cannot be read, it is easy to determine, but if there…
Part Number: ADS8588H Other Parts Discussed in Thread: INA188 , TMUX6219 , OPA2197 , TMUX6236 Dear TI,
We need a programmable Gain amplifier which should have gains of 10 and 50,
input to ADC AD8588H is being fed from current transformer, and we want…
Part Number: ADS8588H Hi,
what is the output voltage of REGCAP1 and REGCAP2? This is not specified in the datasheet, but needs to be clarified for selection of capacitors with appropriate voltage rating.
Regards,
Matthias
Part Number: ADS8588H HI Sir
I want to design a 3 phase meter & poly meter
I choose the ADS8588H for 3 phase monitor---> did you have any source code for Survey?
another project is poly meter-->did you have any suggestion?
thanks
Part Number: ADS8588H Hi,
in the datasheet it's said "In order to maintain the dc accuracy of the system, matching the external source impedance on the AIN_nP input pin with an equivalent resistance on the AIN_nGND pin is recommended"
I wonder how…
Part Number: ADS8588H Hi,
I am doing a tolerance Calculation of a circuit using this ADC. It seems, that the offset error is dominating my tolerance.
I interpret the value of +/-3mV (both ranges) as maximum over operating temperature (-40°C to 125…
Part Number: ADS8588H
hello TI team,
can ADS8588H be set to continous conversion mode, where we don't have to set CONVSTA and CONVSTB each time to signal ADC to convert data and wait for busy signal to go low,
and then reading data from adc ,
…
Part Number: TMS320F28388D I'm trying to use the f28388d to trigger & retrieve ADC data using the two spi channels in THREE-WIRE mode.
Setup:
SPI-C Master - works as expected. SCLK causes the ADC to send data back on DOUTA.
SPI-D Slave:
Same…