Part Number: ADS8588S DOUTA pin only show output value of "0" when reading using SPI protocol.
The configuration of pins are as shown in the attached file.
Steps followed.
1) Setup Serial configuration as shown in the image.
2) Provide 2 Analog…
Part Number: ADS8588S Hi Gent.,
I'm evaluating one DAS design based on ADS8588S, now I have few questions, could you please help on clarifiing them? thanks.
1. For the input impedance descriped in d/s, this is important as it could introduce system…
Part Number: ADS8588S Hi Ti team,
I have selected four ADS8588S to interface 32 sensor data reading simultaneously.
I read data from the adc in parallel mode.
ADC READ procedure that I follow:
Step-1 : Set CONV pin to high. Step -2 Check Busy…
Part Number: ADS8588S Other Parts Discussed in Thread: MUX506 , I am using ADC ADS8588 for multiple channel acquisition with a front end mux MUX506 followed by a high slew rate op-amp AD744. We are finding that a settling time of 60us is required before…
Part Number: ADS8588S There is a place that is not easy to handle in phase, causing the input terminal to become AIN_nP ground, and AIN_nGND is connected to the input single-ended signal. Please help evaluate whether this usage will have adverse effects…
Part Number: ADS8588S
Dear all,
I would like to ask a question about Sampling rate.
In the case of ③, if the sampling rate is calculated from the min value, it will be 66.76 kHz.
There was no indication in the data sheet that there was a delay…
Part Number: ADS8588S Hello,
We have LPC1788 Microcontroller and want to interface with ADS8588S.
So how can we interface ?
And also we need help for sampling rate and digital data reading.
We welcome your suggestions if missing something.
Thank…
Part Number: ADS8588S
Dear,
I am making the DA measure system by ADS8588S chip.
But, I had some problem for sampling rate, please advice this problem
[Test status]
used driver : ad7606.c / ad7606.h / ad7606_spi.c in kernel's default driver…
Part Number: ADS8588S Hi,
Kindly review the board file of ADC designed using IC ADS8588SIPMR .
Schematics and Gerber file is attached. Kindly go through it and let me know your comments.
Regards
Nikhitha antony