Part Number: ADS8638
Tool/software:
Hello,
Referring to the previous thread, I have the exact same question and I fail to understand how figure 71 answers it.
The datasheet says the typical accuracy is 5% of FSR. There are no full scale range specified…
Part Number: ADS8638 Tool/software: Hello,
I'm using this part ADS8638SRGERin a design. I couldn't find anything regarding the exposed pad (EPAD). Does it need to be grounded or left floating?
Thanks
Part Number: ADS8638 Hi,
We are in the process of replacing an ADC in a design which has gone EOL. The TI ADS8638SRGER is an excellent fit, but I was wondering if it is recommended for new designs, or if there is a planned end of life date for this part…
Part Number: ADS8638 Hello~
I have a question about using the ADS8638.
datasheet Page 24. in text => "Whether it is an internal or external reference, be sure to decouple the REF terminal to REFGND with a 10µF capacitor. Place the capacitor close to the…
Part Number: ADS8638 Other Parts Discussed in Thread: TLV4171 Hi,
I am using an ADS8638 in my design to read +/-12V analog signal, it's working good with HVSS = -15V and HVDD = +15V. However I could save some money and space by using a +/-12V power supply…
Part Number: ADS8638 HI!
I have an issue with ADS8638 thru SPI communication
Once I read the register, The IC can't send anything.
is there any problem with schematic or communication control?
Here I attached my schematic.
Thanks
Part Number: ADS8638 Other Parts Discussed in Thread: ADS8668 Hi,
I am using ADS8638, 8 channel ADC for inputs of 0-10V. I am giving 3.3V as supply (DVDD & AVDD) and 10V for HVDD. Is it necessary to give HVSS mux voltage as -10V? Can I give 0V? How is…
Part Number: ADS8638 In page 64 of the DS, the section named "DRIVING ANALOG SIGNAL INPUT WITHOUT AN OPERATIONAL AMPLIFIER" describes the use of a bypass capacitor and the sampling rate for determining the output impedance of the circuit. Can you explain…
Part Number: ADS7138-Q1 Other Parts Discussed in Thread: ADS8638 , ADS8668 , ADS8665 Tool/software: Hello experts,
Can it possible to monitor of the negative power supply's voltage in ADS7138-Q1?
We want to monitor of -3.3V.
Best Regards,
Toru Kimura…
Part Number: ADS8638
Tool/software: TI C/C++ Compiler
Hello Dale,
Sorry for delay in response.
this issue continuation of https://e2e.ti.com/support/data-converters/f/73/t/893830
-As per the SPI MOSI getting Spikes at the end of the 8-bit frame.
1. Is…