Part Number: ADS8694 Other Parts Discussed in Thread: ADS8664 Hi,
We are using ADS8664IDBT in our existing design and planning to use ADS8694IDBT due to higher resolution requirement.
are these chips 1:1 compatible ? I could see pin assignments of both…
Hi Sandeep,
Please see my answers below:
Pin 23 should be directly connected to the AGND ground plane. Please see the Figure 74 in the data sheet.
Pin 22 is a input pin in default condition which is active low power-down, so this pin should be pulled…
Other Parts Discussed in Thread: ADS8688 , ADS8664 , ADS8674 , ADS8684 , ADS8684A , ADS8694 , ADS8668 , ADS8678 , ADS8688A , ADS8698 Hi ti
Could you help to provide some ADC chipset with linux driver(better to have linux source code)? CPU is am571x。
spec
14bit…
Hi Jefferson,
The footprint you showed is not made by TI and it's made by other company, they used ADS8664 pinouts for ADS8668 footprint.
Regards,
Dale
Hi Dale,
thank you for the driver. Now I have a new problem (see screenshot) .
Here is the content of the file:
[ADS8664EVM] ID = "ADS8664 EVM" Resolution = "12" No.of Channels = "4" [ADS8668EVM] ID = "ADS8668 EVM"…
Part Number: ADS8688EVM-PDK Other Parts Discussed in Thread: ADS8688A , ADS8664 , ADS8668 , ADS8674 , ADS8678 , ADS8684 , ADS8688 I am trying to install the software from the micro SD card, but, Windows sees the card as not formatted, so, I can not load the…
Absolutely you can .. you can use the ADS8664 and use the two channels in the way you have described. The ranges for each channel can be configured independent of each other.
Thanks
Other Parts Discussed in Thread: MUX36D04 , MUX36S08 , ADS1248 , INA826 , INA159 , MUX509 , ADS8664 , TVS3300 Hi,
I need to multiplex 4 Analog Input Module for Industrial Outputs to a single A-to-D.
Requirements:
1. Analog Input Module for Industrial Outputs: …