Part Number: ADS8671 Tool/software: Hi team,
I received some questions about ADS8671 from customer. Please support.
1) Datasheet parameter tD_RST_APP is speced 1us max. Does it mean CONVST/CS must be toggled Low to High within 1us after the rising…
Part Number: ADS8671 Other Parts Discussed in Thread: OPA320 I'm trying to count random pulses that cross a negative trigger threshold of -55 mV for only about 25-50 microseconds. The ADS8671 is almost working but it's occasionally skipping pulses.
…
Part Number: ADS8671 Other Parts Discussed in Thread: ADS7142 , ADS8681 I configured the ALARM/SDO-1/GPO pin as an alarm by setting SDO_CTL_REG bits 9-8 to 01b per table 7-14 (SDO_CTL_REG Register Field Descriptions).
I would like the GPIO pin to function…
Part Number: ADS8671 Hello Ti Team,
I am working with the ADS8671 ADC and I couldn't find anything on how the data should be interpreted or what is needed to set up the ADC.
So I have two questions.
1. If I do not write anything to the ADC and…
Part Number: ADS8671
Hello,
When we used the ADS8671 to acquire data, we were acquiring the amplifier amplified signal, the amplifier output +-12.288V signal, Vref=4.096V.
Below is the SPI waveform: adc input voltage range is +-12.288V, Vrefio=4…
Part Number: ADS8671 Hello,
I wasn't able find any information about range switching time of the ADC. When I set the range to new value how long should I wait get reliable readings?
Thanks!
Part Number: ADS8671 Other Parts Discussed in Thread: ADS8900B Hi TI Team,
Thanks for your continuous supporting for my queries.
I am using ADS8671 and ADS8900B in my design.
How can I read the converted data equivalent to the analog signal to be…
Part Number: ADS8671 Dear Expert.
Thank you for your special support everyday.
There is a simple question about ADS8671 IPW.
DS: http://www.tij.co.jp/jp/lit/ds/symlink/ads8671.pdf
What is the slew rate value of PGA (programmable gain amplifier…
Part Number: ADS8671 Other Parts Discussed in Thread: TINA-TI , Tool/software: TINA-TI or Spice Models Hi TI Team,
I am looking for an ADC for measuring 0-5V in 1mV resolution so the required bit is 13. for this requirement I think this part will…
Other Parts Discussed in Thread: ADS8671 , ADS8685 , ADS8689 My design receives a -38V to -60V voltage input over a long cable (100 ft - 300 ft). This board will have an MCU with/without ADC on it. I want to measure incoming negative voltage and communicate…